Part Number: TSB41BA3D Hi,
Currently, customers are using oscillators with a maximum rise / fall time of 4.5 ns.
Since this oscillator is an EOL, customers are planning to use a maximum 6ns rise / fall oscillator.
Does it meet the required clock specifications…
Part Number: TSB41BA3D Hi Team, Our customer would like to see how the TSB41BA3D supply current changes over the temperature range from 25°C to 85°C. The datasheet seems to show the supply current only at 25°C conditions. Do we have data that…
Ignore the G4 suffix.
A/B/D indicate newer revisions. You should get the newest revision (TSB41BA3D), if possible.
I/T indicates temperature ranges.
PFP is the package name.
EP indicates "enhanced products" for military or aerospace applications.…
Other Parts Discussed in Thread: TSB41BA3D I am struggling to find requirements for XI when using an oscillator rather than a crystal.
All documentation and reference designs utilize a crystal, but finding an industrial temperature crystal with the pr…
Other Parts Discussed in Thread: TSB41BA3B , TSB41BA3D , TSB82AA2 We have a design that has used TSB82AA2A and TSB41BA3B for years. We have recently switched to using TSB41BA3D PHY and now the interface does not work. There is apparently a problem in the…
Other Parts Discussed in Thread: TSB41BA3D , TSB41BA3B We would like to confirm that the Product ID for TSB41BA3D is supposed to be 83_30_05. Table 9 on page 24 of SLLS959A contains the same information as the Product ID for TSB41BA3B (Table 7, pg 26, SLLS678…
Other Parts Discussed in Thread: TSB41BA3D , TSB81BA3E Hello,
I am currently working on trying to connect a Raspberry Pi, to the TSB41BA3D physical layer chip. I have a problem with setting this chip up.
In particular, pin 34, CPS, "Cable-power status input…
Hi Jim
We need to clarify between the formatted/packet speed and port operating speed..
When you say sending the PHY packet at S200, we need to understand if this is the formatted/packet speed or the port operating speed. If they are sending the PHY packets…
Part Number: XIO2213B Other Parts Discussed in Thread: TSB41BA3D Hi,
For a new project I want to use the XIO2213B in combination with an external Phy chip. The internal Phy of the XIO2213B will not be used. Is there an application note or reference schematic…