Part Number: TSB43AB23 Hi Team, My customer considers using TSB43AB23 under iTRON OS(operating system). He wants to know if there is standard register setting or sample code for TSB43AB23. Does TI have any information above? Best Regards, Yaita
Part Number: TSB43AB23 Hi Team, I would like to ask about Interrupt Event Register bit18 (regAccessFail). Could you tell me how to handle (debug) when regAccessFail is set "1"? I would also like to know if "SCLK clock signal from the PHY layer" is…
Part Number: TSB43AB23
Dear all,
I would like to ask about read cycle of TSB43AB23.
TSB43AB23 from CPU (Master). (PCL_CLK is set to 33MHz) From the PCI bus side of the CPU, when the single access to the PCI bus space of the TSB43AB23 connected to the…
Part Number: TSB43AB23 Hi team.
My customer are trying to use TSB43AB23 to read the PHY Register.
However, rdDone(b31) did not change to 1 from 0. rdReg(b15) changed to 0 from 1.
(They want to read bit31~bit0.)
In this case, is the lead data sent?
Please…
Part Number: TSB43AB23 Dear, Sir.
My customer is considering to apply TSB43AB23 for their imaging system.
The datsheet defines 0.1uF +- 10% capacitor is needed for these pin.
There is no technical information such as EVM for this product.
They are…
Part Number: TSB43AB23 Hello.
We used TSB43AB23 for Windows 8 PC system got some problem. In Windows 8 device manager can not find IEEE 1994 device. But Windows 10 and Windows 7 is OK.
In Windows 8 had 1394bus.sys and ohci1394.sys files. Please kindly provide your…
Part Number: TSB43AB23 Other Parts Discussed in Thread: TSB41AB3 Hello guys,
One of our customers is considering using TSB43AB23 (IEEE 1394a-2000 OHCI PHY/Link Layer Controller) with TSB41AB3 (IEEE1394a-2000 Three-Port cable Transceiver/Arbiter).
They…
Hello,
To calculate the checksum: take the first byte (address 0x00) and make a sum with the second byte (address 0x01), take the LSB of that sum and then sum that value to the third byte (address 0x02) and so on with all the EEPROM bytes.
Regards.
Other Parts Discussed in Thread: TSB41BA3A , TSB43AB23 , TSB41BA3D , TSB81BA3E , TSB41AB1 Hello,
We have for 1000s of devices used the following network TSB43AB23 <-> cable <-> (port 1) TSB41BA3A * mode 8, pmc mode, bmode (port 2) -> TSB17BA1 …