Hello Takumi,
See my answers to your questions below:
Q1) You are correct. The only difference between the two is that the TSC2046E has enhanced ESD protection.
Q2) ESD information for TSC2046 :
HBM: 8kV
CDM: 1kV
MM: 200V
As for the TSC2046E , it…
Hi Leila,
You could have a look at the following devices: TSC2014, TSC2007 and TSC2004. They could fit in your application.
Best Regards
José Luis Figueroa
Application Engineer
Other Parts Discussed in Thread: TSC2014 , TSC2017 , TSC2007 , TSC2003 Hi,
I would like to select a touchscreen controller with I2C interface and 4-wire input, plus pressure sensing ability. The selection tool filtered out the following results.
I looked…
Hello,
There is no specific layout requirement for touch screen controller (or ADS7846) with the GQC package, and just follow the common practice and the layout guidance provided in the TSC's d/s.
Additionally, for your reference only, attached is an…
Other Parts Discussed in Thread: TSC2014 , TSC2004 , TSC2017 hello,
May I know if TI has not touchscreen controller that come with hardware filtering like , Microchip part, p/n: AR1020?
for Example refering TSC2014 Is the pre-processing stage consider…
Hello Jeff,
Because the issue occurs during weak touch (not solid strong touch), I still think you should consider the suggested sequence for reading touch data, where please also note the PD0 setting in each of the reading command.
In TSC2046 (and in all…