I would suggest to put capacitors to ground very close to IC pins and IC ground. Then i would ask to do the test and if issue gets resolved then removing capacitors one by one till we have the minimum needed.
For example: A single 1u cap on the 3 pins…
Hi Sanjay,
I will send you the circuit of touch-panel and the measurement enviroment.
The test results in 1) and 2).
Is this an abnormal condition?
[circuit]
[Pictures around the IC]
The red arrow shows TSC2017.
[ measurement enviroment ]
The product…
Part Number: TSC2017 Hi all,
I would like to know the conditions for the PENIRQ Pin goes to Low.
I understand that one condition is when the panel is touched.
What conditions will it be forced to Low?
Best Regards,
Ryusuke
Part Number: TSC2017 Hi all,
I would like to know the results of IEC61400-4-2.
Which of a) to c) does it apply?
a) The device works normally when the voltage of the target is applied.
b) The device malfunctions, but it does not stop working.
c) Operator…
Part Number: TSC2017 When Vdd = 0V, the voltage range that can be input to the C1 (SDA) and D1 (SCL) pins is -0.3V to Vdd+0.3V, or ±0.3V, is this correct? If I were to pull up with an external 3.3V, would the semiconductors be damaged?
Part Number: TSC2017 When Vdd = 0V, the voltage range that can be input to the C1 (SDA) and D1 (SCL) pins is from -0.3V to Vdd+0.3V, or ±0.3V, is this correct?
If I were to pull up with an external 3.3V, would the semiconductors be damaged?
Part Number: TSC2017 Hi TI expert,
It seems that TSC2017 don't give the ACK feedback signal, could you please help analysis the possible cause of the issue? For more detail information, you can contact me through email.
B R,
Jayce Luo
Part Number: TSC2017 Other Parts Discussed in Thread: TSC2007 Tool/software: Linux Please help me to provide the TSC2017 driver file under the Linux system,thankyou!