Other Parts Discussed in Thread: TSC2014 , TSC2017 , TSC2007 , TSC2003 Hi,
I would like to select a touchscreen controller with I2C interface and 4-wire input, plus pressure sensing ability. The selection tool filtered out the following results.
I looked…
Other Parts Discussed in Thread: TSC2017 When Hardware Reset or Software Reset is carried out, is weight time required by the time it accesses TSC2017 after reset release? Or is immediately after reset release to access possible?
Hello Takumi,
See my answers to your questions below:
Q1) You are correct. The only difference between the two is that the TSC2046E has enhanced ESD protection.
Q2) ESD information for TSC2046 :
HBM: 8kV
CDM: 1kV
MM: 200V
As for the TSC2046E , it…
Naoki,
I was able to get the information you are requesting - it took some time to collect all relevant design/ application details.
Unfortunately, the TSC2007 does *not* have a software reset.
Any TSC2007 customer will have to meet the POR requirements…
Hi Al,
Welcome to our e2e Forum. I'm curious, have you looked over the application notes found under the TSC2017 product folder? That would be a good place to start. My understanding is that R Sense is only needed when you want to implement multi…
Part Number: TSC2046 Other Parts Discussed in Thread: TSC2017 , ADS7845 , TSC2013-Q1
Hi all Would you mind if we ask TSC2046? Is it possible to use two coordinate detection function? Should we use TSC2017 instead of TSC2046? Or, does ADS7845 correspond for…
Hi José,
I'm trying to calculate the x,y coordinates in Linux. I have the TSC2007 driver.
When I put the $ dmesg | tail in My terminal:
] usb 5-2: Product: Unknown ] usb 5-2: Manufacturer: Unknown ] usb 5-2: USB disconnect, device number 8 ] usb…
Hi José,
The real time communication is possible with USB-MODEVM Interface and TSC2017 driver?
Do you have the VI model of TSC2017EVM for LabView?
Thanks,
Leila