Part Number: TSER953 Hi Team,
I am using below mentioned poc circuit. I have some questions regarding that poc circuit.
My requirement for PoC circuit is:
Current= 500mA
Temperature rating= -20'C to 55'C
Frequency: 25MHz to 2.1GHz
Query 1:…
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 Hi,
We have used TSER953 and TDES954 for 1920x1080p60 RAW10 video in the past successfully.
Now we are doing 3840x2160p30 RA10 and having an issue. Frame sync broken and sometimes partial frames…
Part Number: TSER953 Hi Team,
I am using TSER953 part for CSI2 single lane mode.
Can you please tell me the current consumption for using only single lane.
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 I have CSI-2 with 600Mbps/lane and 4 lanes on TSER953 input port. I configured the TSER953 trough des TDES954. TSER953 is on RX0. i2c addr tdes: 0x68, i2c-addr tser: 0x30. i2c transfers:
-->…
Part Number: TSER953 Hi Support Team
I am planning to use OSC and CLK Generator for CLKIN.
So I was wondering if you could give me the input specifications for CLKIN. I am wondering how many ppm will be required.
Best regards.
Hello,
The pixels are relevant to determining if a certain camera can be supported. In the equation,
Video Throughput = HActive x VActive x (Frame Rate) x Bits-Per-Pixel x Overhead (Assume 25% if unknown)
HActive refers to the number of horizontal active…
Hi Oba,
Thanks for following up here. Regarding sample code, there are a number of different code examples within the datasheets of the TSER953 and TDES960 which can help the customer here. These are primarily included in the detailed description section…
Part Number: TSER953 Hi Support Team,
I am using MIPI CSI-2 1lane with TSER953. I want to switch the CSI-2 port for AW design reasons. Is it necessary to set registers?
I am thinking that I should connect only the port I want to use and leave the other…
Part Number: TSER953 Hi Support Team,
According to Table 7-7, Clocking Modes, CSI BANDWIDTH varies depending on REF FREQUENCY(f),
but I think that Mipi data rate (per CSI-2 lane) will not change from MAX832Mbps even if REF FREQUENCY(f) varies.
Is this…
Part Number: TSER953 Hi Support Team
I would like to confirm FC DATA RATE and CSI BANDWIDTH.
From Table 7-7, Clocking Modes, when the internal clock is 24.2 MHz in CSI-2 asynchronous mode, the following is correct. FC DATA RATE :24.2×80=1.936Gbps…