Part Number: TSW30SH84EVM Hello,
I have two TSW1400 boards with TSW30SH84EVMs connected to them. I am currently trying to synchronize the outputs so they are in phase. After reading the documentation provided here I was wondering it is feasible on…
Part Number: TSW30SH84EVM
Can you please elaborate the use of CLK4 & CLK5, CLK6 & CLK7, CLK8 & CLK9 in the context of tsw30sh84evm? Also, what is the function of the "divider"?
Sure no problem.
Fdac = 1G
Interp = x2
Data rate = 500M
First lets do some math to figure out our divider values.
The VCO will only output frequencies within the range 2750M -3072M. The signal outputted by the VCO will need to be divided down…
Hello Ken,
In this forum post we spoke about several example dll and automation code including labview examples for the TSW30SH84. Also you emailed me matlab automation which was helpful. I was wondering is there anyway you could send me the LabView…
Hey Dan,
This is so great thank you very much this is really helpful, what I meant by without the use of external reference is lowering the data rate as you have but without any use of J12 on the TSW30SH84EVM. So to clarify I am asking how to lower…
Acknowledged that you are not getting the proper output. Let's step back a bit.
Can you get a proper output with just engaging the "Constant Output"? This will verify that the DAC device is set up properly and that the modulator is working as expected…
Part Number: TSW30SH84EVM Hello,
I was just wondering if I could get a general tutorial or some sort of guidelines to setting up two TSW30SH84EVM synchronously with one or two TSW1400.
Thank you,
Joshua Johnson