Part Number: TSW38J84EVM Hi, I am using the TSW38J84EVM and I would like to know if there is any easy way to reset the board to its initial state when I first power it up. When the board is first powered it draws around 945mA. I would like to reset it…
Other Parts Discussed in Thread: LMK04828 , TRF3722 Hi all,
I am using TSW38J84EVM and I would like to configure the external clock capabilities.
As explained in the EVM user guide I want to operate the LMK04828 in the clock divider mode by supplying the…
Other Parts Discussed in Thread: TIDA-00409 Hello Team,
I have a customer who is requesting Altium files for the TSW38J84EVM. They want to base their design off it. Could you please for ward the Altium files for the TSW38J84EVM if available.
Thank you…
Hi all,
I am using TSW38J84EVM and I would like to configure the external clock capabilities using the LMK0428, which so far is not working.
I have introduced my question yesterday in High Speed Data Converters Forum in topic with the name "TSW38J84EVM…
Other Parts Discussed in Thread: DAC38J84EVM , TRF3722 Hi all,
I am using the TI Tx board TSW38J84EVM together with the TSW14J56EVM pattern generator board.
I am using the DAC3XJ84_LMF_841 image file for the TSW14J56 , and the DAC is also configured to work…
Hi Gordon,
My contact at Soshin mentioned that he had contacted you already. Perhaps you missed his email? I will private message you offline and provide his contact information.
-Kang
Hi all, i have the following Eval Boards connected
- TSW14J56EVM (Rev. D) - TSW38J84EVM (Rev. B)
and i am trying to set them up like it is described in the TSW3XJ8XEVM User Guide in Chapter 4. But i see no output Signal an the Spectrum Analyzer. What i…
In the schematic package for both the TSW38J84 EVM and for the DAC3Xj8X EVM, there seems to be something strange about the signal labelling on the page marked "DAC" (for both EVMs). This appears to be the same schematic page copied for both EVMs. The…
Loganathan,
1. Correct.
2. Correct
3. No. There is an option to sum path A with path C and path B with path D but this is only available with the DAC38J84, which has 4 DAC's. You cannot use this option with the DAC38J82.
You need an external modulator…
Jim, > When SYNC goes low at higher temps, is it staying low? No, when SYNC gets low it gets high after a while, then it can go low again and so on. > Is the FPGA sending the K28.5 characters during this time? Yes, when SYNC goes low then FPGA starts…