Part Number: DAC38RF82 Hello,
I am trying to use TCM2-33WX+ as it has a low phase and amplitude imbalance.
On TSW40RF82EVM , I have made the following mods.
1. populate L7, L8, R382 and R380.
2. remove R381 and R386.
3. Connect J40 TCM2-33WX+ secondary pin…
Hello Jim,
can we use an external balun with TI EVM? I would like to use TCM2-33WX+ as it has low phase and amplitude imbalance.
On TSW40RF82EVM, will the following mods work?
1. populate L7, L8, R382 and R380.
2. remove R381 and R386.
3. Connect J40 TCM2…
Hi Carlos,
The TSW40RF82EVM has both an ADC and DAC on the single eval board. The outputs/inputs of the board are however single ended but you can use an external balun to convert it back to differential for testing. The board also has an FMC connector…
Part Number: TSW14J56EVM Hi, I am using a TSW40RF82EVM card with the configuration 2T2R_RevC_ConstInput_6xDec_12xInt_2949p12M_5898p2_4915p2Gb connected to a TSW14J56EVM card. I generate on the DACs a succession of frequencies separated by zeros that I…