Part Number: TUSB1210 Hey team,
I have an application that does not have a VBus in the design. In our datasheet we call out that the "TUSB1210 does not strictly require VBUS to function." However we do not specify if it should be left open, grounded,…
Part Number: TUSB1210 Hi,
My customer wants compliance test of USB2 Host on TUSB1210BRHB.
To do compliance test, what setting of TUSB1210 do they need to do?
Please advise us.
Thanks and best regards, M.HATTORI
Part Number: TUSB1210 Hi team,
In TUSB1210 datasheet, the power up sequence is specified in Figure 6-1. But from my understanding, the power up sequence is not mandatory as the internal leakage should not be significant as discussed in the thread below…
Part Number: TUSB1210 Hi TIer
Could we can control the TUSB1210 to continue send the DUT test waveform to help customer test Eye diagram?
in some code? or what is the method?
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB1210 hi Team
Customer uses TUSB1210 to hang out of the FPGA with ULPI interface inside the FPGA to interface with TUSB1210, TUSB1210 to connect to the PC, would you like to ask if additional…
Part Number: TUSB1210 Hi,Team
Our TUSB1210 circuit configuration is configured to supply 3.3V from an external DC-DC power supply to VBAT and VDD33.(Figure1) Please tell me how to mount the VBAT and VDD33 capacitors of the TUSB1210.
◇Figure1
【question…
Part Number: TUSB1210 Other Parts Discussed in Thread: SN74AXC4T774 , TXU0101 , 2N7001T Hi,
We are using TUSB1210BRHBR for USB to ULPI interface. Kindly provide your suggestions for the below questions.
1.We are performing for Host, device and Host OTG configurations…
our FPGA board has FPGA chip + TUSB1210 chip.
and inside FPGA, I have USB device RTL code.
so Device ( FPGA ) <--> TUSB1210 in a single board .
Device input signal was shared to u.
so what is expectation from TUSB1210 ?
I think it try send out…
Part Number: TUSB1210 Hi,
We are using TUSB1210BRHBR in our design for USB to ULPI interface, which is interfaced with FPGA. For REFCLK input, it is mentioned as to provide external clock source. The clock source requires 3.3V as per datasheet and we…
Part Number: TUSB1210 Other Parts Discussed in Thread: SN74AXC4T774 Hi,
We are using TUSB1210BRHBR in our design for USB to ULPI interface, which is interfaced with FPGA. For REFCLK input, it is mentioned as to provide external clock source. The clock…