Part Number: TUSB1211 Since TUSB1211 is EOL, I would like you to introduce an alternative product.
The function I want to realize is to charge the device (tablet) while realizing OTG using the ACA (BC1.2) standard.
If possible, I would like you to introduce…
Part Number: TUSB1211 Hi expert,
As TUSB1211 is going to EOL, could you please recommend another TI device to replace it? It would be perfect if we have P2P devices. Thanks.
Jared
regards.
Part Number: TUSB1211 Team,
Can you please direct me to some details on how to connect TUSB1211A1ZRQ and TM4C129ENCPDT signals related to USB-OTG operation. Specifically both the processor and the transceiver have connections for the ID and the VBUS inputs…
Part Number: TUSB1211 hello
we want to convert UART data to USB host interface.
can we use TUSB1211 to work in USB host mode to connect USB device IC??
Thanks!
Part Number: TUSB1211 Hi,
What is the difference between TUSB1210 and TUSB1211? I can not understand the difference.
For example, In the "description" of TSUB1211 data sheet page1, "USB Battery Charging Specification Ver 1.1 Support".…
Part Number: TUSB1211 Hi,
I have simple question regarding TI's USB transceiver chip.
Is TUSB1211 device supported by WEC7 OS as standard? I would like to know what TI USB transceiver is supported by WEC7.
Because, as you know, WEC7 is old Windows CE…
Part Number: TUSB1211 Team,
My customer is questioning the internal PLL jitter performance, which is not listed in the spec.
If they supply REFCLK in with 19.2MHz clock, and the clock phase noise is
-90dBc@10Hz, -100dBc@100Hz, -110dBc@1kHz,-125dBc@1MHz…
Part Number: TUSB1211 HI Sir
1. If I would like to use TUSB1211 for Linux OS ,I don't need to install any driver ,is it right ?
2. Due to I saw SMSC solution register is not the same with TUSB1211 ,May I know TUSB1211 have reference code can let…
Part Number: TUSB1211 Hi team,
The TUSB121X USB2.0 Board Guidelines document, Section 3.02, says that ULPI interfaces should have equal path lengths to have equal delays. I'm curious to know, is there a spec to how much delay variation the interface…
Part Number: TUSB1211 We have the TUSB1211 designed in and are seeing some production fallout related to bus errors on the ULIP bus.
I am trying to do a margin analysis and I need to know what the minimum output delay time (TDD, TDC) is for this part…