Part Number: TUSB1310
Hi, how can I find the IBIS AMI model of TUSB1310 which is a USB 3.0 transceiver. I need this model to use in Hyperlynx simulation. I guess TUSB1310 is quite old device and support up to 5 Gbps. Do we have any newer version of the…
Part Number: TUSB1310A We are develop a USB HUB. We tested our RTL in FPGA and using ULPI PHY, TUSB1310A(USB3_HT3 made by E-ELEMENTS) with HAPS DX7 board.
But we found high-speed detection handshake is not successful. When USB device send TX CMD (84 45…
Part Number: TUSB1310
I have some questions regarding USB 3.0 Transceiver.
1- The PIPE interface between MCU and the USB 3.0 Transceiver in Figure 1-1 in datasheet. The PIPE interface is 16 bit wide 250 MHz. This interface is Single Data Rate (SDR). Does…
Part Number: TUSB1310 Hello TI,
As the website indicates, this part is not suitable fore designs. We tried searching USB3 transceivers, could not find any on the website, however it lists the part numbers for USB hubs.
Do you have any other USB3 transceivers…
Part Number: TUSB1310 Hi Team,
there are several questions on below power up sequence requirement.
1. what does the grey means in VDD1P1 ( blue) ?
2. what does the dotted line means in Red?
3. can OUT_ENABLE and RESETN be power up at the same time?
…
Part Number: TUSB1310 which all registers will be programmed by USB controller for PHY to be up and running ?
what is the initialization and configuration procedure for PHY.
Any manual/guide will be appreciated.
Thanks & Regards,
Amarnath
Part Number: TUSB1310 Hi,
We supplied 5V with vbus pin, and we made reset signal to tusb1310.
And checked pwrpresent pin, but pwrpresent pin was low.
Let me know the reason or solution.
Thanks,
Doohan
Part Number: TUSB1310A Other Parts Discussed in Thread: TUSB1310 Hi, Ti Support team,
I am working on a USB3 project that is basic on TUSB1310A chip and
my question can be description as below
Does TUSB1310 can be operating on both host and device side…
Part Number: TUSB1310 Hi,
We are using add on board from E-Elements which is based on TUSB1310 chip.
We are testing USB 3.0 Host controller solution.
TX_DETRX_LPBK is getting asserted from Host controller side.
In response PHY_STATUS is getting asserted…
Hi Nishie:
We use these parts for all our USB3 devices with TUSB1310, but I don't have layout example for TUSB1310.
C0603X5R0J104M for 0.1uf
CC0201KRX7R7BB103 for 0.01uf
Regards
Brian