Part Number: TUSB1310A Hi team,
customer met a problem as below
sequence as below
pull 1V and 1.8V low then pull up 1.8V, pull up out_enable, pull up 1.1V, pull up resetn. phy_mode is 1, refclksel is 3 setting 40MHz on XI. But then receiver has no response…
Part Number: TUSB1310A Hi
W'd like to implement usb 2.0 host controller on xilinx fpga(VCU118) using htg_fmc_usb30_board (attached tusb1310A) !
We supply external 5.V using power supply to VBUS pin on TSUB1310. and we checked pwrpresent pin whether…
Part Number: TUSB1310A Hi,
I received a question from a customer.
1. I am experiencing 8 b/10 b Decode Errors, are the following posts relevant?
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/631769/tusb1310a-tusb1310a-fpga-rx…
Part Number: TUSB1310A Now that USB 3.0 in devices ares becoming more prevalent. there is increasing need to support it in embedded designs.
Any plan for TI to bring a solution (that can be use for NON-PCI design) back into the product line and make it…
Part Number: TUSB1310A Hi experts,
When I connected our USB device with TUSB1310A to some of the hosts with legacy Intel chipsets, C612 and C620, BER were not good at exp -8 to -10. However it was fine with recent chipsets. And other USB devices, such…
Part Number: TUSB1310A Other Parts Discussed in Thread: TUSB1310 Hi, Ti Support team,
I am working on a USB3 project that is basic on TUSB1310A chip and
my question can be description as below
Does TUSB1310 can be operating on both host and device side…
Part Number: TUSB1310A Hello,experts:
I have a question toward this TUSB1310A, coudl this chip support the dual role port function? could I use this transceiver to support the host device and otg mode or just device mode?
thanks a lot
Part Number: TUSB1310A Other Parts Discussed in Thread: TUSB1310
Hi Experts,
Seeking your assistance on this query from a customer:
We are using add on board from E-Elements which is based on TUSB1310 chip.
We are testing USB 3.0 Host controller solution…
Part Number: TUSB1310A We ran into the same issue like below . May I know how below issue is resolved ?
TUSB1310A: Intermittently Stays in Electrical Idle When Instructed to Go into Transmit Data Mode - Interface forum - Interface - TI E2E support fo…
Part Number: TUSB1310A At present, when we use E-ELEMENTS' USB3 daughter board (including TI PHY: TUSB1310A) to debug, we find that the clock state output by phy is abnormal. T he test situation and the questions to be consulted are summarized as follows…