Part Number: TUSB216 Hi,
Is the USB host able to connect to D1 and USB connector connects to D2? Or it must follow the following connection as below picture?
Best regards,
Randy
Part Number: TUSB216-Q1 Other Parts Discussed in Thread: PMP30338 I design for automotive, I follow PMP30338 reference design. I'm thinking of using tusb-216q1 considering in-vehicle cabling. But for wiring losses, should I position the tusb216-q1 in my…
Hi Shirakawa-San,
Thank you for the patience. What is the desired Vcc? Please refer to Input RX_SEN in Electrical Characteristics of the datasheet as below. Note that low level input voltage is 0.75V and high level input voltage is 75% minimum and 5.5V…
Part Number: TUSB216 ・RX_SEN
Can you tell me what I can configure?
RX_SEN Levels are High, Medium, and Low. For example, High is how the signal is set?
・BOOST
Can you tell me what I can configure?
BOOST Level is 0~3. For example, how does Level 3 set…
Part Number: TUSB216-Q1 Other Parts Discussed in Thread: TS3USB221A-Q1 We are looking into use of the TUSB216-Q1 re-driver but I see a confusing detail on the TI webpage. With 480Mbit High Speed USB data rate, how could the bandwidth be 240MHz? Also,…
Part Number: TUSB216 Other Parts Discussed in Thread: , TUSB213EVM , TUSB217A , TUSB213 , TUSB217 Hi,
We tried running compliance test with TUSB216 (in device mode) but the eye diagram looks exactly the same no matter what the gain settings were. I read…
Part Number: TUSB216 Other Parts Discussed in Thread: TUSB211 , Hi team,
my customer want to use TUSB216 to be 2sd of TUSB211,
if they don't have any scenario that will disable redriver during power on, can they just float the RSTZ pin with a cap? …
Part Number: TUSB216-Q1 Other Parts Discussed in Thread: TUSB216 , TUSB217A hello expert,
For TUSB216-Q1 BC1.2 CDP function, if CDP_ENZ=L, VCC is stable, what are the possible reasons of fail BC1.2 handshake?
We found the if CD pin is asserted earlier than…