Part Number: TUSB217-Q1 Hi,
Because the working voltage provided by our circuit to tusb217-q1 is not fixed, the range is 2.75V ~ 3.85v, and the voltage will change with the product working temperature (± 0.2V). Do the gain/sensitivity and other states…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217EVM Hi team,
does the TUSB217-Q1 have USB-IF authentication, Can you share the report? thanks.
Part Number: TUSB217-Q1 Hi team,
Our customer wants to estimate the maximum power consumption of TUSB217-Q1, but the static current is not given in the datasheet. Do you have a more accurate estimation method ? how to give further guidance to the customer…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: DXP , Hello Team,
Thanks for your every support. I got some questions from customer as below. Can you provide answers?
Q1. Regarding with DxP/DxM internal circuit, Is the D1M and D2M were DC isolation…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217 Hi Sir,
We checked TUSB217 d/s found there are different comments for R setting.
Pls kindly check which one is correct, thanks.
RBOOST = 1.69K or1.8K?
R1 = 47K or 37K ?
R2 = 24K or 47K ? …
Part Number: TUSB217-Q1 Hello Team,
Thanks for your support.
Let me ask some question about RSTN pin of TUSB217-Q1.
Q. Are the 500kohm PU and 1.8Mohm PD still active regardless device functional mode(LS mode, FS mode, HS mode, High speed down stream port…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217 Hi Sir,
Would you pls advise if TUSB217 either D1 or D2 can be HOST?
If yes, how to define which side is HOST? Thanks.
Thanks, Ian.
Part Number: TUSB217-Q1 Hello Team,
Thanks for your support.
I have some question about TUSB217-Q1
Q. In non I2C mode, can we left SDA pin Open? Or do we need any pull-up/pull-down?
Q. The VCC range is wide (2.3V~6.5V). Dow the VCC voltage level affect…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217 Dear Sirs,
My customer had some question about D+/D- input signal level in HS mode!
If customer input signal is diff. with +/- 200mV range (0~200mV and 0~-200mV) to TUSB217, will TUSB217…