Part Number: TUSB320 Tool/software: I am trying to design a system that connects an iPad to a ADC/DAC through a USB-C Port. The iPad can be either a source of a sink to power the 5V bus based upon if a Power Supply is connected. The iPad should always…
Part Number: TUSB320 Other Parts Discussed in Thread: , ESD441 Tool/software: Hello , for TUSB320 and similar parts, VTH_DFP_CC_USB is listed in the datasheet Rev F as from 1.51V to 1.64V. I also see the default pullup current of 80uA +/- 20%.
If I understand…
Part Number: TUSB320 Tool/software: Hi,
My customer is using the TUSB320 to detect current capability from the source, however they've realized that the device does not support CC communication along with detecting the pull up on the source.
Can…
Part Number: TUSB320 Tool/software: Hello:
May I ask if TI's TUSB320 supports the EU new regulation EN IEC 62680-1-3?
Customers need to evaluate and select a TYPE-C control switch that supports the EU new regulation EN IEC 62680-1-3. The chip performance…
Hi Ohad,
Is there a USB-C port at the USB hub? The TUSB320 needs to communicate with CC lines in order to operate, so if there is a type-c port on the hub so that it can communicate with the type-c on the phone, then I believe it should work there, yes…
Part Number: TUSB320 Other Parts Discussed in Thread: TPS65987D
Tool/software:
looking for a simple solution to the following.
I have an iPad and my device encased in a sealed housing.
permanent USBC cable runs from iPad to my device to power my de…