Part Number: TUSB320 Tool/software:
What is the max output current of USB TYPEA?
How to set the output current of USB TYPEA?
Is there anyway to set the output current of USB TYPEA below 100mA?
Part Number: TUSB320 Other Parts Discussed in Thread: TUSB422 Tool/software: Team,
In PV Inverter that has a DEVICE side with TYPE-C application, which is very simple function needed. I don't prefer to add the related circuitry to the PD protocol, in…
Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320 Tool/software: I am facing USB C-to-C compatibility issues with some laptop brands. I am using the TUSB320HA device with the Port pin left open to select DRP mode by default. I am experiencing…
Part Number: TUSB320 I'm using TUSB320 configured as DRP and I'm finding that (when nothing is connected to the USB-C connector) the ID output keeps oscillating between high and low at approximately 1Hz. Presumably this shouldn't be happening? I'd expect…
Part Number: TUSB320 Tool/software: Hi,
My customer is using the TUSB320 to detect current capability from the source, however they've realized that the device does not support CC communication along with detecting the pull up on the source.
Can…
Part Number: TUSB320 Tool/software: I am trying to design a system that connects an iPad to a ADC/DAC through a USB-C Port. The iPad can be either a source of a sink to power the 5V bus based upon if a Power Supply is connected. The iPad should always…
Part Number: TUSB320-HA-EVM Other Parts Discussed in Thread: TUSB320 , TPS65987D , TPS65987 I am currently testing the TUSB320.EVM. We require DFP, UFP, DRP and to be able to swap Sink and Source positions. Specific to our case we are trying to achieve…
Part Number: TUSB320 Other Parts Discussed in Thread: TPS25751 , TPD4S201 , TPS25751EVM , TUSB422 Tool/software: Hello, My customer would like to develop a product being connected to a Host PC or a Tablet via USB-TypeC. For USB data, PC or Tablet is DFP…
Part Number: BQ25895 Other Parts Discussed in Thread: LM2596 , TUSB320 , , BQ25985 , PMP4451 , BQ25890
Tool/software:
Hello, my board currently has the following power stage:
LM2596, to drive main +5V rail from external 12V battery
LM2735X,…