Part Number: TUSB320-HA-EVM Other Parts Discussed in Thread: TUSB320 , TPS65987D , TPS65987 I am currently testing the TUSB320.EVM. We require DFP, UFP, DRP and to be able to swap Sink and Source positions. Specific to our case we are trying to achieve…
Part Number: TUSB320-HA-EVM Other Parts Discussed in Thread: USB2ANY Hi TI expert
I would like to know if I can use USB2ANY to configure a TUSB320-HA-EVM board.
Best regards,
Thomas
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hello forum,
After many hours of debugging drv8353s.c and SPI read halts ADCC1 interrupt there were several issues encounterd with the release code UMCSDK v5.03 and v5.04. The worst…
Part Number: F29H85X-SOM-EVM Other Parts Discussed in Thread: C2000WARE Tool/software: Hi,
if activated it doesnt compile even after including driverlib.h.
please let me know if it is needed or not.
BR
Muhammad
Part Number: TUSB320 Hello: I am a new E.E. quite new to touch Type-C USB design, what I try to do is first to have EVM of TUSB320 to figure it out. But I have found that there are TUSB320-EVM, TUSB320-LA-EVM and TUSB320-HA-EVM. I am confused that what…
Part Number: TPS1685EVM Tool/software: Hello,
Just wondering about this - the datasheet has 3.3V as pullup voltage using 33k-ohm resistors and the EVM has a 5V pullup with 10k resistors - does either work or is +5V w/10k preferred?
Just wanted to…
Part Number: TMDS181 Tool/software: Hi team,
I saw the users guide of TMDS181 (sllu228a): https://www.ti.com/lit/ug/sllu228a/sllu228a.pdf
There is a description below. Have this bug fixed in new GUI already?
Regards,
Hayashi
Part Number: TLK2711EVM-CVAL Tool/software: Hello.
EVM board has pull-up, while device has internal pull-down at PRBSEN.
If EVM board Jumper does not installed, PRBSEN voltage is 1.7V.
( 2.5 V * 10k / (4.7k + 10k) )
Intermediate voltage is not…