Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M04 , ADS131M08EVM , , ADS131M04EVM , ADS131M08 Hi team
Does it have EVM? Or, I can use ADS131M04/06/08EVM? Which part is the most similar to M02?
Thanks
Ricky Lau said: Are you using AM64x and AM243x via UniFlash GUI?
Yes, I was using the GUI. The Uniflash GUI recognized the board and listed it correctly. When I select a board, it responds the same with AM64 and AM243. But when I attempt to load/run…
Hi Xulin, Estimating the effort in debugging and identifying the root cause, the current plan from TI is to target for a fix in SDK 9.1. I checked internally, and currently there are no plans to provide an intermediate patch.
I shall get back to you…
Part Number: TDA4VM Hi Team,
Single board silkscreen J721EXSJG01 EVM to boot Linux or RTOS operating system from SD card with serial interface information as follows:
COM1: Information is printed, only Hex values, but cannot be entered
COM2…
Part Number: AM625 Hi E2E Team,
EVM SK-AM62x has pin E7 as "TEMP_DIODE_P" and NC into design while into AM62x processor datasheet has pin E7 as "MCU_RESETz" for ALW package. Please let us know your thoughts on the same.
Regards,
Aditya
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: SK-TDA4VM , AM69 , SK-AM69 , TDA4VH
Hi,
Do you have a TDA4VH-Q1 EVM which has a 12-layer or 10-layer stackup like SK-TDA4VM?
The current TDA4VH-Q1 EVM https://www.ti.com/tool/J784S4XEVM has…
Part Number: AWRL1432BOOST Other Parts Discussed in Thread: SYSCONFIG Hi, TI Team,
I run the MCAN External Read Write example on my xWRL1432 evm following the instruction as the link below. But PCAN has Bus warning after PC sent a CAN FD message to…
Part Number: TUSB320-LA-EVM Other Parts Discussed in Thread: TUSB320EVM , TUSB320 Hi team
Regards to TUSB320LA-EVM, I have below problems need your help to clarify. Thanks!
As TUSB320 datasheet mentioned below, UFP mode can support Accessory…
Part Number: AWR2243 Other Parts Discussed in Thread: MMWCAS-RF-EVM Without MMWCAS-DSP-EVM, has any output interface on MMWCAS-RF-EVM? (USB、UART、SPI or I2C)
If not, how to get the data if I don't use the mmwave studio?