Hi TI,
Issue1 - Pending: i am trying to enable .l2dmemory in the c7x core linker file(ti-processor-sdk-rtos-j721e-evm-08_02_00_05_lin_evm/vision_apps/platform/j721e/rtos/c7x_1/j721e_linker_freertos.cmd) which is required in our vision_apps/apps/basic_demos…
Thanks, Nick!
Now I have a USB access to EVM.
Regards,
Jani
laboratorio@laboratorio-ThinkPad-T410s:~$ picocom -b 115200 -f n -y n -d 8 -p 1 /dev/ttyUSB1 picocom v2.2 port is : /dev/ttyUSB1 flowcontrol : none baudrate is : 115200 parity is : none databits…
Part Number: USB-CTM-MINIDK-EVM Other Parts Discussed in Thread: TPS25750 , TPS65982 , TPS65988 , TUSB320 , TUSB320LAI Hi, i want to design USB_C hub,
it's have 3 ports
1. USB_C connected to tablet (Host)
2. USB 3.0 type A connected to Device
3. Power…
Nick Saulnier said: Did you add the resource table to your linker.cmd file, as documented on that page you linked to? I do not see a resource table section in your linker.cmd file.
Refer to section "Update the linker.cmd file" https://dev.ti.com…
Hi Pranay,
TUSB320 does not have internal FW that can be changed, it is a state machine based device. Could you share the test log for review? In your VIF file Type_C_Supports_Audio_Accessory should be listed as Yes to reflect support for accessories. …
Weird, I can't reply to you directly.
So I did all you suggested. SPI is dead, NPOR on IC STATUS is 0, in fact everything is 0. My LA tells me this.
you can see some small spikes on MISO, but I think they're just noise.
I swear I had this weird…
Part Number: BEAGLE-3P-BBONE-AI
Hi team,
My BB AI is running: ti-processor-sdk-linux-rt-am57xx-evm-06.03.00.106
I want to enable UART 10 support (on Header Connector 9 of the board)
I had configured the pinmux & enabled UART 10 through dts file (am5729…
Hello,
You are correct the common EVM uses W35 not the similar W25. The CMM and the flasher as configured only use a common subset of features. As such, the file can be used for either part. However, the erase block size should be set depending on the…
Part Number: TUSB320 Hi, we are using the TUSB320 evaluation board and everything seems to work fine when we connect the devboard to a laptop or to a Type-C power adapter. The CURRENT_MODE_DETECT (i2c register 0x08) and the ATTACHED_STATE (i2c register 0x09…
Hi Hemant:
Let me introduce the history about the psdkla\visonsdk\qt\weston
We're begin with visionsdk3.04&3.05 as it not support the QT, we copy the QT 5.6 from the psdkla 3.x from the local FAE,and QT works well with weston, but this visionsdk not…