Hello,
The cTI20 provides pins for JTAG, Power/Ground, trace, trigger and control signals. The cTI20's EMU0-4 signals can be used for control, trace, or trigger between a TDA4 and a Lauterbach debug system. The TI reference board/EVM uses a larger MIPI…
Do you have an evaluation board/kit EVM?
Figure 2 is from legacy that is to show a rough concept and may not be regarded/used as actual implementation; the actual implementation could be more complex than it.
Main purpose of the RLD is to drive a voltage…
Bonjour, malgré mes relances par différents moyens (mail et support client) on me dit que cela devrait maintenant fonctionner, à chaque fois, mais j'en suis toujours au point de départ: Je n'ai QUE I2C dans PPC3 et j'ai seulement Purepathcontrol dans…
Hi Jerome,
The default diodes populated on the EVM are only meant to solely power TUSB320 and basic operation of the TUSB320 (cable detection, TUSB320 I2C read/writes etc.) If you are looking to do actual charging through the EVM the diodes do need to…
RamPrasad,
I found that one and that is the one I am using. I have added a sensor entry and the bsp.
I added some missing I2C6 support and changed the LCD info to match our LCD displays.
Everything is compiling until linking. It gives me errors with…
Part Number: TRF372017 Other Parts Discussed in Thread: LMX8410L ,
Hi Teams,
I am studying TRF372017 and LMX8410L to build a transciever.
There are several questions as below which I can't find the answers from datasheets or relative documents, or just…
Hi,
Jay Sun said: 1) What arguments I have to pass in " make -s can_app " command to compile code just for J7200?
You can replace the BOARD with j7200_evm. Run the below command:
make -C build/ BOARD=j7200_evm can_app -s
Jay Sun said: 2) In SDK…
Part Number: TDA4VM hi
Ask for help
We use 2 tda4-evm boards to test the SGMII feasibility on the PORT 2 (SERDES 0 Lan1) with SDK V7.2.
I reference resources https://e2e.ti.com/support/processors/f/processors-forum/936840/faq-dra829vxevm-is-it-possible…
Hello, which configuration file are trying to use? Here are list of specific instructions I used to build AM64x SDK:
wget https://developer.arm.com/-/media/Files/downloads/gnu-a/9.2-2019.12/binrel/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar…
Hi,
Let me fill in some gaps here. When configured as a DFP the data role for the USB-C port should be a USB Host however you have a the US port of a USB Hub connected. This will be in conflict with the smartphone which most likely operates a DRP. The…