Part Number: TUSB320EVM Other Parts Discussed in Thread: TUSB320 Dear Sir,
May I know, if TUSB320 EVM can work in DFP mode with 5V adaptor attached then output 3A from typeC port?
My customer did some testing with EVM but still fail to get 3A from…
Hi,
Unfortunately you will need a PD controller of this kind of application. Having Data and power following in opposite directions requires a Power Role swap or Data Role swap for your Type-C port. TUSB320EVM (Type-C controllers) can be used in cases…
Hi Timoteo,
I recommend implementing your type-C port as a debug accessory. As a debug accessory you are allowed to use all other pins for different purposes other than the standard USB-C usage. You can refer to Appendix B in the Type-C specification…
Part Number: TUSB320EVM Other Parts Discussed in Thread: TUSB320 In a new product design, I have a USB Full Speed peripheral on custom hardware, which will connect to a cell phone with a USB-C port.
It must operate in one of two modes.
Mode 1: Phone…
Is there any more support needed for this issue? If so please reply with any relevant details so that I can further assist you. For now I will be marking this thread as "TI Thinks Resolved". If you have resolved your issue, please post the solution to…
Hi Zack,
I believe this is correct function as i understand it. D9 and D11 should be installed depending on where you would like power to come from. D11 should be installed by default so the Type-C port is powered by the DC 5V jack or Micro USB port…
Part Number: TUSB320EVM Other Parts Discussed in Thread: TUSB320 Hi,
I am using TUSB320EVM for testing purpose. Please let me know the method to configure CSR registers of TUSB320 IC when EVM is connected to PC through microAB port J6 via USB-A to Micro…
Matt,
I used the TUSB320EVM with my Dell Latitude laptop and was unable to reproduce your issue. Could you please measure the voltage on the CC pin during operation and let me know what you see?
Thanks,