Part Number: TUSB4041I Hi,
Does TUSB4041I have any HW pin can control LED?
My customer want let LED enable when TUSB4041I Down port is during read/write.
Thanks!
Jeff
Part Number: TUSB4041I Hi
I'm designing USB HUB application with TUSB4041I, and I refer to the schematic of TUSB4041I EVM.
I have a question about USB connector shell connection.
What is the purpose of pin8 connected to GND through RC in parallel…
Part Number: TUSB4041I Other Parts Discussed in Thread: TPS2000C Hi TI Team,
We are using a USB HUB Device "TUSB4041IPAPQ" in our Design. Where we are planning to use the Device without any external Programming (Non-Programmable). As per the datashee…
Part Number: TUSB4041I Dear Specialists,
My customer is considering TUSB4041I and has a question.
I would be grateful if you could advise.
---
Could you please let us know the minimum capacitor of VDD(1.1V)
According to the datasheet P.36 10.1 TUSB4041I…
To summarize this issue for future reference,
The TUSB404x has a designed workaround triggered by older versions of Windows. Before Windows 8, the standard Windows driver for hubs would send multiple resets downstream during enumeration in order to support…
Part Number: TUSB4041I Hi experts!
Could you please tell me what to do with the unused terminals of TUSB4041I?
This circuit is designed with reference to the evaluation board. Is there any problem with the following?
Best Regards
Part Number: TUSB4041I Hello Team,
as we don't have a 7 port hub in our portfolio could I use 2 TUSB4041I and connect the 2nd to one output of the 1st to get 7 outputs?
Thank you and best Regards, Hans
Part Number: TUSB4041I-Q1
HI,
I developed my pcb with TUSB4041 (it is based on reference design from TI). Unfortunatelly after connecting it to Raspberry Pi Zero W 2 it is not recognized as usb-hub but 'vendor specific class'. To the chip an eeprom is…
Part Number: TUSB4041I Other Parts Discussed in Thread: TUSB8041 Dear Specialists,
My customer'd like to obtain OTP tool for TUSB4041I.
Could you please provide?
I appreciate your great help in advance.
Best regards,
Shinichi
Part Number: TUSB4041I Dear Specialists,
My customer encountered similar trouble.
Could you please let us know the way to PWRCTL1/BATEN1 high?
---
I powered on the TUSB4041 with the following configuration. However, the output of PWRCTL1/BATEN1 did not…