Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: TUSB8020B Hi,
So I need to use connect an EEPROM to set above modes, right?
Can I set above modes on our EVM?
Thanks.
Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: TUSB8020B Hi Sir,
My customer wants to use TUSB8020B-Q1 on their project and they need Linux driver for Linux kernel v5.10.72 and v5.15.5. Do we have a driver for TUSB8020B-Q1?
Part Number: TUSB8020B-Q1 Hi,
If customer doesn't configure 8020 by EEPROM nor SMBUS, just use its default settings, no power switching control needed, no charger, can it work as a two ports USB3.0 hub? Thanks.
Part Number: TUSB8020B-Q1 Dear team,
USB 3.0 specs doesn't define the max cable length. Someone said that the max length is better to be smaller than 3m. Does our device will impact the length? What is our experienced length value?
Thanks & Best Regards…
Part Number: TUSB8020B-Q1 Hi team,
I would like to ask that do we have such similar automotive level device with HSIC function to beat the following competitor's device? Thank you.
C710013CYFU0000_USB3503.pdf
Part Number: TUSB8020B-Q1 Hi,
I am using TI USB hub having part number "TUSB8020BIPHPQ1" in my design. I am not able to find its layout files and guidelines on Website. Please share if your have any reference design for this device.
Regard…
Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: TUSB8020B Hi team,
I would like to force my TUSB8020B-Q1 to communicate in USB2.0 mode with any USB peripherals even if that support USB3.0.
Could you advise how to configure the device to force…
Part Number: TUSB8020B-Q1 Hi TI Team,
Our Customer is using the TUSB8020B-Q1 HUB in the custom design. It has one non-removable device connected to the downstream port 1 and one type A (removable device) port on downstream port 2. It is currently connected…
Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: TUSB8020B Hi,
Currently we have issue whereby the host is not able to detect the TUSB8020B hub. We already check the connection:
- power up sequence is correct - 3.3V up before 1.1V
- USB_VBUS…