Part Number: TUSS4470 Other Parts Discussed in Thread: BOOSTXL-TUSS4440 , CSD88537ND , PGA460 Hi,
is there a circuit recommendation to drive the TUSS4470 with external mosfet/transformator to drive a 100W transducer?
The 12V battery voltage is available…
Hi Michael,
If you are only seeking to measure the water level, then I do not recommend the old TDC1000. The TDC1000 is a two channel ultrasonic IC; you only need a single channel ultrasonic IC.
Depending on your ultrasonic application use-case, we…
Hi John,
Depending on whether you are attempting to make a flow measurement or a concentration/identification measurement, there are a few options available.
If you need to know the flow rate, then the MSP430FR6047 is the best option.
If you need…
Sajjad,
Thank you for your inquiry. The intended use of TUSS4470 is to be able to drive an ultrasonic transducer for variable number of pulses at the resonant frequency of the transducer.
Can you provide any information on the specifications for your…
Paulvanna,
For education purposes, attached is the zipped firmware for the TDC1000-7200EVM: TDC1000_7200EVM Firmware Official Obsolete.zip
It is true that this EVM has been obsoleted, so we can no longer new support TDC1000-7200EVM request. Depending…
With the size of systems decreasing day after day, and increasing demands for power efficiency often times we get asked about power consumption for PGA460 and TUSS44x0. This can be somewhat of a difficult question to answer because the power consumption…
Hello, Thank you for your question and detailed description.
The issue is that the iron wall will significantly attenuate the ultrasonic signal for the transmit and echo return.
This is a figure from our Ultrasonic Sensing Basics app note , displaying…
Other Parts Discussed in Thread: PGA460 , TUSS4470 , MSP430FR6047 , TUSS4440 , BOOSTXL-PGA460 , BOOSTXL-TUSS4470 , EVM430-FR6047 , BOOSTXL-TUSS4440 , TDC1000 , TDC1011 Ultrasonic sensing uses the propagating sound waves at a frequency above the range…
Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: MSP-EXP430F5529LP , TUSS4470 , TDC1000 , TDC1000-Q1 , BOOSTXL-TUSS4470 BOOSTTXL-TUSS4470 vs. TDC1000-C2000EVM:
1. Is the ultrasonic received data in EVM BOOSTTXL-TUSS4470 (or in TDC1000…
Other Parts Discussed in Thread: AFE5809 , AFE5808A , TX7516 Hi, I am designing an Ultrasonic flaw detector for metals. Ultrasonic flaw detector uses high-frequency sound waves (ultrasound) to detect and evaluate flaws or defects in materials, such as…