Other Parts Discussed in Thread: AM3517 , TCA6416 , TVP5146 Hi All
I am working on customized board based on AM3517evm.
I am using PSP 04.02.00.07, i have successfully modified the code of board-am3517evm.c and included driver for SX8652 in kernel…
Hi Prashanth,
filesave is working fine in the DM36x EVM. Also streaming is also working. But webGUI is not working. We have changed in the rcS file according to the YUV Sensor Integration Guide which describes how to run application in the EVM.
For…
Hi Anuj,
I tested the code by commenting these lines. Still Live video stopped on the first frame. Streaming is working fine. And webpage is opening.
Here is the boot logs:
Fullscreen
boot_log_24_08.txt
Download
DM36x initialization…
Other Parts Discussed in Thread: TVP5146 Hi All:
I runing encode demo with dvsdk_demos_2_00_00_07 in dvsdk_2_00_00_22, But system no respond after capture and encode some frame, It seems the DSP hand after runing with CE_DEBUG=2 Lots of error message…
Other Parts Discussed in Thread: DM3730 , ADS7846 , TVP5146M2 , TVP5146 Hi,
I am working on DM3730 Mistral EVM. I am trying to run the video loopback application from composite input(CVBS) to LCD output. I am using DVSDK_4306 - Linux 2.6.37
For this…
I have been using DVSDK 2.xx for months and recently upgraded to DVSDK 4.00. On our EVM DM356 board the system boots fine.
Today I installed DVSDK 4.01 (dvsdk_dm365-evm_4_01_00_09_setuplinux). Followed the instructions (ie ./setup.sh) and on power…
Other Parts Discussed in Thread: TVP5146 i don`t know this issue.
anyone help me.
r7 = C004ED84 r6 = C0B1C5A0 r5 = 00000000 r4 = C5626000 [<c0053968>] (do_exit+0x0/0xda0) from [<c003b6a8>] (die+0x350/0x3a0) [<c003b358>] (die+0x0/0x3a0) from [<c003dcec…
There is a MUSB issue on AM3517EVM with AM35x-OMAP35x-PSP-SDK-03.00.01.06.
After power the 3517EVM, then insert a USB device without power (mouse, mass storage or powerless hub), linux can enumrate USB device correctly. then remove the device, system…
Hi Prashant,
Actually I am working on the quality of live video and streaming video.
For the live video: capture, dei, resize, display threads
1. I checked the resolution in capture thread, resize thread, dei thread and display thread. May be…
Other Parts Discussed in Thread: DM3730 , BQ27200 , WL1271 , OMAP3530 , TVP5146 , AM3517 Hi,
I am using DM3730 processor, ov2643 2M pixel camera. when I run the application "VIDIOC_STREAMON: Broken pipe" occurred. After kernel log I attached the C video…