Other Parts Discussed in Thread: TVP5160 , TVP5150 , THS8200 , TVP5147 , TFP403 Hi,
I'm looking for video converter IC's for my application and not able judge and select the IC's. please assist me to pick the right one.
BR
satya
Part Number: TVP5146M2 Other Parts Discussed in Thread: TVP5160 Good Morning,
I'm using TVP5146M2 in my project and I'm having problems with image quality.
The defect is especially noticeable around the text. Please look at the following pictures…
Better comb filter.
You can look at the TVP5147 and TVP5160 which provide better comb performance but are more expensive.
The TVP5160 will give the best performance but is a 3D comb filter hence also requires SDRAM for frame storage.
ADC resolution…
RGB + Syncs is not NTSC, it is VGA.
What resolution is the output?
Your best option is the TVP7002 for digitizing YPbPr and RGB+S signals. For single wire NTSC or S-Video you can use the TVP5150, TVP5151, TVP5146, TVP5147 or TVP5160 depending on the quality…
Other Parts Discussed in Thread: TVP5150AM1 , TVP5160 , TVP5146 , TVP5147 I am developing an UVC solution using TVP5150AM1. I am successfully getting NTSC video but there are color issues. When there's white text on black
background visible amount of…
Other Parts Discussed in Thread: AM3505 , TVP5160 , PCM1804 The Linux(Linux-2.6.32-psp03.00.01.06) is hanging up on AM3505. I would like to know why the Linux is hanging up.
[Hardware] - AM3505(600MHz) I2C-1: Temperature Sensors(AD7415), RealTimeClock (S…
Muhammad Salih said: any other camera is used as SPI slave in this platform?
I can provide you the below pointers:
I don't believe DM816x can accept analog video directly. I believe it will need an external video decoder such as the TVP5151, TVP5146/7…
Your options for 525p are the TVP5160 and the TVP7002.
The TVP5160 is actually a high quality 3D comb filter but can be used in 2D mode without the SDRAM which will result in lower quality decoded CVBS video.
The TVP5160 can also decode all the CVBS standards…
I understand that your system is not an EVM but since I do not have your setup I can only use similar hardware. My test DOES only test the TVP5160.
On the EVM the TVP5160 does NOT hold the I2C lines low when in PD mode. this clearly indicates that the…
Other Parts Discussed in Thread: TVP5150AM1 , TVP5158 , TVP5146 , TVP5147 , TVP5160 , TVP7002 In TVPxxxx list, only TVP5150AM1‘s status is active.But TVP5150AM1 input interface is only composite analog video, can't support component video.
TVP5158 status…