Hello,
I'm trying to setup a VGA/XGA/SVGA video capture using the DM648 EVM. Has anyone done this before?
I understand that the TVP7000 digitizer interfaces to the DM648 using only a 16 bit Y/C data path. And since the TVP7000 doesn't perform the…
Other Parts Discussed in Thread: THS8200 Hi all,
I check the download files of THS8200 register setting for 1080p, but the description about 1080p50 was wrong.
The content mentioned "TVP7000', not THS8200..
I have tried content as listed…
RIFAT BENVENISTE said: Below is the RGB transformed image I captured by CCS As its seen there are some green dots on the word vivident and also there is a blue colored noise on the dark regions of the image
Assuming the image is getting into the DM6437…
In order to make dm355 ipnc support for VGA singals ,we have linked tvp7000 to the vpfe module of dm355.Now ,we have problems as follows:
1 The video's colour we have obtained on the internet is abnormal .The original black backgrounds becomes blue…
Other Parts Discussed in Thread: TVP70025I , TVP7002 , SN74LVC2G17 Hi
I designed a VGA to LVDS convertor board with TVP70025I and SN65LVDS84AQ to connect a 10.4" TFT ( NL10276BC20-04 , it is a XGA LCD=1024x768 60hz ) to VGA port ( 1024x768 60hz ) of…
Other Parts Discussed in Thread: TVP7002 , THS7353 , THS7303 , THS8200 , CDCE949 , LMH1980
I want to add 1080p30 h264 encoder demo on the TI DM6467T EVM board.
but TI only provided 720p30 h264 encode demo on the TI DM6467T EVM board.
I know that TI have…
720p display is part of the sample application HD Loopback found if location <pspdrivers_1_XX_XX>\packages\ti\sdo\pspdrivers\system\dm648\bios\evmDM648\video\sample.
By default this sample application captures a 1080i 60Hz from TVP7000 and displays…
Below are TVP7002 settings that should work for 1280x1024 SXGA60Hz, 4:2:2 YCbCr out with embedded syncs. The TVP input MUX settings may not be configured correctly for your board. You will need to use a processor that supports a 108Mhz input pixel clock…
Thanks, I did find that doc, but there aren't specific details as far as mux settings. Your tip did lead me back to the BSL code, though, where I found this #define EVM_ECP_VIDEO_MUX_REG (0x06) // ECP Video Mux register #define EVM_ECP_VIDEO_MUX_VP…
Bernie,
Try the settings below for this format. It is not clear what the total pixels per line are for this format. The settings below are based on a camera found that specified 768 active and 811 total pixels/line. This may requrie adjustment for your…