Part Number: TX517EVM Dear TI Employees,
Following the user manual, I have set up our TX517EVM. After power up, I try to show the output 1 and 2 on our oscilloscope (our oscilloscope is capable of receiving 200Vpp signal). However, I cannot see any results…
Part Number: TX517EVM Other Parts Discussed in Thread: AFE5809EVM , , TX810 , TX517 Hi,
We have made a fully functional sonar system using the following EVMs:
TX517EVM -> Transducer -> TX810EVM -> AFE5809EVM -> TSW1400EVM
Here is a photo of our…
Part Number: TX517EVM Hello,
Following the user manual, on P1-Header of TX517EVM, there is no ground. However, I can see that there is ground on J1-Header. We're using P1 header. Do we need to connect the ground? If yes, where should we connect our ground…
Part Number: TX810EVM Dear TI Friends,
We would like to create a sonar transmit and receive system. Here is our final goal : TX517EVM -> xdcr -> TX810EVM-> AFE5809EVM->TSW1400EVM. However, at this stage I would like to verify the system without using a…
Part Number: TX517EVM Dear TI friends,
I can see a USB interface connector (J6) on TX517EVM. I was wondering what is the functionality of this USB interface. Also, is it possible to configure the board through this usb connection? If yes, do you have any…
Part Number: TX517EVM Dear TI Family,
On TX517EVM -> J1 header, I found that the mark indicator, which is shown below is probably wrong. As you know, we usually use a dot indicator on headers to indicate Pin 1. However, the dot indicator on this board…
Hello again,
We are still looking for a method to change the output frequency of TX517EVM to 400Khz or 800Khz. Would it be possible to control this board externally?
We were thinking to generate PWM wave using our OMAP L138 LCDK, and then give this…
Part Number: TX517EVM Dear Friends,
I would like to use TX517EVM as our Transmitter and I have the following two questions:
Is it possible to configure this EVM over an SPI connection? For example, using an SPI connection to set the register values. …
Part Number: TX517EVM
Dear TI Employees,
We have recently purchased TX517EVM. Following the user manual, we've connected +5v and ground to TX517EVM. The following image is from the user manual. However after powering up, the Z1 (ZENER DIODE) becomes…
Part Number: TX517EVM Other Parts Discussed in Thread: TX517 Dear TI Family,
We're using TX517EVM. I would like to know what is the minimum current required for each power supply pin. Specifically, Pins VAA, LV0, and HV0. These pins require +2.5 V, -1…