Part Number: TX7316 Tool/software: Hello E2E Experts,
Good day.
I have a question about the TX7316 TR_EN pin. If I use on-chip beamforming, doesn't the level of the TR_EN* pin matter? Is it just the register bits that control its turn-on and turn-off…
Part Number: TX7316 Hi Team,
Regarding the TX7316 D/S, could you please share your insights for the below questions? Thanks.
1. There is a T/R switch for TX7316 device, do we have a typical application BD to show how to set up with some end-equipment such…
Part Number: TX7316EVM Other Parts Discussed in Thread: TX7316 Hi team,
Because there is no schematic and PCB layout files of TX7316EVM found on ti.com.Can you share schematic and PCB layout files of TX7316EVM, which can be used to customer PCB design…
Part Number: TX7316 We have designed the TX7316 into a multibeam sonar system. The system has two 8-channel transducers, of which only one is operated at a time. We are using the T/R switch to multiplex from the 16 pulser channels down to 8 receiver channels…
Part Number: TX7516 Other Parts Discussed in Thread: TX7316 Hi,
Let me confirm one point for sure about TX7516.
We can replace TX7316 with TX7516 directly, correct?
Thank you for your support.
Best Regards,
Takumi
Part Number: TX7516 Other Parts Discussed in Thread: TX7316 Hi,
Let me ask you the basic question.
What is the difference between TX7516 and TX7316?
I do not understand the difference, only package??
Thank you for your support.
Best Regards,
Takumi
Part Number: TX7316EVM Other Parts Discussed in Thread: TX7316 Hello,
I recently bought the TX7316 and TSW1400FPGA board. I would like to ask if the TSW1400 can be used to control the transmission and reception of the TX7316 pulse signal. If so, what interface…
Part Number: TX7316 Hi ,
TX7316 can't work and make a pulse with off-chip beamforming mode,
HV is +/-5.5V ,AVVDD is 1.8V ,
connect both BF_CLKP and BF_CLKM to ground,
TR_BF_SYNCP/M to ground,
RESYNC=0, LVL_3Z_5 to ground 3 level mode
IN_A1_0/IN_A1_1…