Part Number: TX7316EVM Other Parts Discussed in Thread: TX7316 Tool/software: Hello,
I have recently purchased a TX7316EVM. I am using it 5 level mode. I am trying to generate a 10MHz 4 pulses signal. I tried many options in "Profile configaration" but…
Part Number: TX7316
Hi team,
I would like to check if TX7316 can be used in LCD tester application. Can TX7316 support below use cases?
1. AC output: +-50V peak-peak square wave, 50% duty, the frequency range is from 10kHz to 1.5MHz, the load is a 1nF…
Part Number: TX7316 Hi,
Datasheet reccomends to use 2x0.27uF caps on each FLOAT*_HV_* pin. Can I use instead 1x0.47uF or 1x0.56uF (rating 10V)? If yes, which capacitance value TI reccomends?
Best Regards,
Mariusz
Part Number: TX7316 Hi Team, Our customer is requesting for the power values information for the 3-Level mode of TX7316 below if available: In receive-only mode: In transmit-receive mode: In CW mode (0.6-A mode): In global power-down mode: Only the 5-Level mode…
Part Number: TX7316 Hello,
My customer has a question about Initialization Sequence in On-chip Beamforming mode in TX7316.
[Background]
* The initialization sequence in On-chip Beamforming mode is described in D/S (SLOS950B) P.120 to 121.
The step 5…
Part Number: TX7332 Other Parts Discussed in Thread: AFE5832LP , TX7316 , AFE5809
Dear TI experts,
My customer looked reference SBOA361 for their new project. It includes TX7332 and AFE5832LP. And they have some questions about it. could you check the…
i think it is called as 4A_Mode_CNTRL_1/2 . hope it helps. i will ask our datasheet team whether we can fix that.
by the way, TX7316 is in produciton now:)
Part Number: TX7516 Other Parts Discussed in Thread: TX7316 Hi,
1. Should SEN be held low between the two SPI cycles required for the read operation?
i.e Will two normal SPI reads with SEN going high between the cycles not work?
Please clarify.
2. Is…
Hi,
In the user guide of TX7316 EVM, the initial current number and voltage expected in different nodes are mentioned. Can you cross check if your setup matching these numbers?
TX7316 and TSW1400 are independent setups. First you can try to bring up TX7316…