Part Number: TX7332 Other Parts Discussed in Thread: TX7516 Hi,
I would like to ask you a question about the difference between TX7332 and 7516.
What is the main difference betwen the devices?
I suppose the difference is "ch number" (32/16) and "current…
Part Number: TX7332 When connecting two TX7332 to a single AFE, what state must the second TX7332 be in? Our board design works find with one TX7332 installed, but as soon as we solder in the 2nd TX7332, no pulse is measured on the output pins (of the…
Part Number: TX7332 Dear,
I am currently using the on-chip beamforming mode of TX7332 to conduct experiments. At present, by controlling the pulses of TR_EN and TR_BF_SYNC pins, a switch closing signal can be captured once. But I want to control the switch…
Part Number: TX7332 Hi there,
I would like to use the TX7332 for a large signal drive, In the datasheet it says the current limit is from 1.2A to 0.3A, I am wondering what is the max output voltage with those current limits. Could someone help me to find…
Part Number: AFE5832LP Dear engineers, We have got Swaroop board and installed the HSDC Pro and AFE5832LPTX EVM,and realized the data collection. Now we looking forward to design a Ultrasonic imaging system. We plan to make some changes on existing Swaroop…
Part Number: TX7332 Hello. We are using the TX7332 in our sonar application. Can you provide any 'C' source code examples on controlling this unit? We are mainly looking at Frequency/pulse length programmability. We do already have an NDA with you for…
Part Number: TX7332 We have a custom PCB using the TX7332 IC mated with a Xilinx Ultrascale+ processor. In protoyping, our +/-5 supply is causing issues with the boot sequence of our low voltage rails and we cannot test the Xilinx chip. One (temporary…
Part Number: TX7332 Hi,
Let me ask you a question about the current drive ability of TX7332.
According to the datasheet, there describes that TX7332 can drive 1.2A(typ).
Is this value means "per ch", correct?
That is to say, can this device…
Part Number: TI-EMAIL-ORDERING Other Parts Discussed in Thread: TX7332 , AFE5832LP Dear Sir/Madam,
My name is Marcos Alepuz, Managing Director of Fertoolity SL ( https://fertoolity.com/en/ ), a company that works on development of hardware and software for…
Hi Cherry,
Please refer to the "Programming" section in the datasheet of TX7332 for information regarding the SPI read and write. This is same for both on-chip and off-chip beamforming modes.
Regards
Savyan