Part Number: TX7332 Hello. We are using the TX7332 in our sonar application. Can you provide any 'C' source code examples on controlling this unit? We are mainly looking at Frequency/pulse length programmability. We do already have an NDA with you for…
Part Number: TX7332 Hi TI we are developing a new ultrosound product using TX7332s +AFE58JD48s. and we have some questions with these two chips: 1、the active T/R switch in TX7332 can be controlled with PIN_EN_TR and TR_EN_n, but each PIN_EN_TR will affect…
Part Number: TX7332 Hi,
Let me ask you a question about the current drive ability of TX7332.
According to the datasheet, there describes that TX7332 can drive 1.2A(typ).
Is this value means "per ch", correct?
That is to say, can this device drive…
Part Number: TX7332 We have a custom PCB using the TX7332 IC mated with a Xilinx Ultrascale+ processor. In protoyping, our +/-5 supply is causing issues with the boot sequence of our low voltage rails and we cannot test the Xilinx chip. One (temporary…
Part Number: TX7332
Hello
In the data sheet it is mentioned that "TI strongly recommends" using Clock and Sync in the same manner, meaning both SE or both Diff.
Following that, a note mentioning this is a MUST.
I accidently didn't put both on…
Part Number: AFE5832LP Dear engineers, We have got Swaroop board and installed the HSDC Pro and AFE5832LPTX EVM,and realized the data collection. Now we looking forward to design a Ultrasonic imaging system. We plan to make some changes on existing Swaroop…
Part Number: TIDA-010057 Hi,
Could you please help me to get the full support documents of the Swaroop design? We are working on a wearable US device prototype and planning to use the same transmit and receive ICs used in Swaroop design.
Also, I would…
Part Number: TX7332 I have two TX7332 connected to an AFE, sharing channels. I want to pulse on one TX7332, but switch off the TR_Enable for the duration of the acquisition. Similarly on the 2nd TX7332, I want to switch on the TR_Enable for the duration…
Part Number: AFE5832 Other Parts Discussed in Thread: TX7332 , , Hi Sir/Madam,
We are developing a hand-held ultrasound and are using AFE5832LP together with TX7332. We are now on the stage of developing color-flow imaging with autocorrelation. However…
Part Number: TX7332 Hi Experts,
Good day! I need your assistance as we can not see any information regarding the BSDL for this device.
Can TX7332 support boundary scan? If yes, Could you please share the details and the BSDL file?
Thank you in advance…