Part Number: TX7516 Tool/software: Hello,
We have been working with TX7516 to transmit various electronic patterns for an ultrasound device.
In a peculiar manner, we discovered that a pattern that should be valid is not being transmitted correctly (only…
Part Number: TX7516 Other Parts Discussed in Thread: TX7316 Hi,
1. Should SEN be held low between the two SPI cycles required for the read operation?
i.e Will two normal SPI reads with SEN going high between the cycles not work?
Please clarify.
2. Is…
Part Number: TX7516 Other Parts Discussed in Thread: AFE5828 Hi
For thermal dissipation, metal heatsink will be mounted on the top TX7516 . We should apply adequate mechanical pressure to ensure good thermal conductivity.
What is the recommended Mechanical…
Part Number: TX7516 Other Parts Discussed in Thread: TX7316 Hi,
Let me confirm one point for sure about TX7516.
We can replace TX7316 with TX7516 directly, correct?
Thank you for your support.
Best Regards,
Takumi
Part Number: TX7516 Other Parts Discussed in Thread: TX7316 Hi,
Let me ask you the basic question.
What is the difference between TX7516 and TX7316?
I do not understand the difference, only package??
Thank you for your support.
Best Regards,
Takumi
Part Number: TX75E16 Other Parts Discussed in Thread: TX7516 , Hi,
Let me ask you a basic question about the difference between TX7516 and TX75E16.
I suppose the differnece is only following thing,
"Programmable load damp resistor: 200 Ω, 100 Ω or 67"…
Part Number: TX7516
Hi there
we are noticed that 75E16 is better than 7516. one of the main advantage is better elastography support.
We also found "low glitch" in 75E16 datasheet, could you pls help explain what is this? seems not much info in 75E16…
Part Number: TX7332 Other Parts Discussed in Thread: TX7516 Hi,
I would like to ask you a question about the difference between TX7332 and 7516.
What is the main difference betwen the devices?
I suppose the difference is "ch number" (32/16) and "current…
Part Number: TX7516 Hi TIer
Since the customer did not use Dynamic Power Mode, he configured DIS_DYN_PDN_LDO to 1, but found that color noise appeared on the central axis of the sector image (phased array ultrasound, color mode, sector scanning). We…