Part Number: TX810EVM Other Parts Discussed in Thread: TX810 Dear TI Employees,
I've already read the manuals of TX810 and TX810 EVM. I would like to know in more details what this board does, and why do we need this board. Any general information about…
Hello guys,
I am confused that how to connect an ultrasound probe to AFE58xx device. Is it possible to connect directly AFE58xx to an ultrasound probe????????? (I do not use transmit beamformer and high-pulser)
Should I use Transmit/Receive switch…
Other Parts Discussed in Thread: TX810 , TS12A4516 , TS12A44514 , TS5A9411 Hello,
I'm working on an ultrasound transducer driver. I'm currently using the TX810, and the transducer in this project is a CMUT ship. The output signal of the CMUT ship is…
Other Parts Discussed in Thread: TX810 Hello,
I want to ask if TX810 can use +5V single power supply. What's the difference between double and single power ?
Thank you.
David Kei
Other Parts Discussed in Thread: TX810 Hi,
Currently we're designing a small ultrasound device for development and research. We are interested in using TX810. In our system high-channel count or power consumption aren't most important factors, so we…
Chandu,
The control switches only control the bias current through the switch to control the output pulse amplitude. There is no timing control needed with the TX810, you do not need to time the transmit mode and receive mode because they are the same…
Other Parts Discussed in Thread: TX810 , LM96570 , AFE5808 Sir,
I am working for portable ultra sound system design.
How the working of TX810 IC is controlled with B1/B2/B3 control inputs.Such that the switch will off in transmit mode and on state…
Other Parts Discussed in Thread: TX810 Does the tx810 have bias current control input internal pulldowns or pullups?
There is a figure 15 in the data sheet showing pulldowns that I believe indicates they are external, but I would I like make sure since…