Part Number: TXB0101 Other Parts Discussed in Thread: TXU0101 , SN74LXC1T45 VCCA=3.3V, VCCB=5V, OE=3.3V. A 50kΩ pull-down resistor is connected to A of TXB0101. 3.3V system is connected to CPU. The speed is 100kHz. It will not work if connected to a 5V…
Part Number: TXB0101 Other Parts Discussed in Thread: TXS0101 Hello team,
TXB0101 and TXS0101 are similar device and bypass cap should be placed on both VCCA and VCCB. But bypass cap is placed on TXS0101EVM and not placed on TXB0101EVM.
Is TXB0101 wrong…
Part Number: TXB0101 Hello team,
Customer want to use TXB0101 which support 1.8V and bidirectional level shifter. Their usage is that both VCCA and VCCB are 1.8V but TXB0101 must follow the condition of VCCA<VCCB so I'm not sure their usage can meet…
Part Number: TXB0101 I have a product where pins VCCA, OE and A are linked to connector pins. Normally VCCA and OE are connected (through the connector) to 3.3v power, and A receives a 3.3v serial signal. This all works perfectly.
Now I want to connect…
Part Number: TXB0101 Other Parts Discussed in Thread: LSF0101 , SN74AXC1T45 Hi,
can two TXB0101 be connected in series or what would be a suitable solution to connect a 1V8 system bidirectionally to the input of a 3V3 TXB0101?
Thanks and regards,
Man…
Part Number: TXB0102
Hi,
May I know what is the VOH and VOL level of TXB0102 level translator
We wan to know for VOHB and VOLB, Since its given blank in the datasheet.
Regards,
Nireeksha
Part Number: TXB0101 Other Parts Discussed in Thread: TLV740P , SN74LVC1G17 Hi team,
My customer need an unidirectional level shifter to transfer 3.3V to 1.8V. However, they only have 3.3V supply on board. I read the TXB0101 datasheet and I think it could…
Part Number: TXB0101 Other Parts Discussed in Thread: PCM1864 , , SN74AXC1T45 Hi Sirs, As title, can we drive two 24576MHz, 3.3V MCLK to PCM1864 without a clock buffer as the block diagram below? The input current of the PCM1864 is +/-10uA, while we failed…
Part Number: TXB0101 Hi Team,
I am using the TXB0101 in a bidirectional level-shifting/buffering application but requires both enabling and disabling the buffer according to various needs.
Can I hard short the OE pin to ground and VCCA for enabling and…
Part Number: TXB0101 Other Parts Discussed in Thread: SN74AUP1T157 , SN74AVC4T245 , , TXB0104 Regaridng the High/Low Level Input Voltage on the Recommended Operating Conditions, the value is VCCI/0V respectively.
If the Undershoot is observed and the voltage…