Part Number: TXE8124-Q1 Hi, TI Experts
Question 1: as picture shows below , Is there Clamp Diode between GPIO Pin to VCC ?
( Does the IC has the ability to clamp the input voltage to VCC+04V?)
Question 2:
If all the IC GPIOs are used for GPO…
Part Number: TXE8124-Q1 Other Parts Discussed in Thread: TXE8124 , TIC12400 , TIC12400-Q1 , hi,Expert
What is the voltage level when TXE8124 CS is high ? high impedance?
What is the voltage level when TIC12400 CS is high ? high impedance?
For…
Part Number: TXE8124-Q1 Other Parts Discussed in Thread: TCA6408A Tool/software: Hi,
Is it possible to get the IBIS model for TXE8124-Q1 ? If no model available can you please recommend a similar part?
Thanks and regards,
Cantaloupe
Part Number: TXE8124-Q1 Tool/software: Hello,
Is there a minimum hold time that output data on the SPI bus for this device is defined? Would this parameter be tV (SDO)? I see a maximum is defined, but we would need to confirm the minimum data hold time…
Part Number: TXE8124-Q1 Other Parts Discussed in Thread: TXE8124 , Tool/software: hi,
A question about TXE8124 latched output.
1. how to understand this sentence " Latched outputs with high-current drive maximum capability for directly driving LEDs…
Part Number: TXE8124-Q1 Other Parts Discussed in Thread: TXE8116 , TXE8124 Tool/software: FAQ: Logic and Voltage Translation > IxC and SPI >> VOH/IOH/VOL/IOL and Total ICC Current Definitions
This FAQ describes 6 key spec's for I/O expanders.
These…
Part Number: TXE8116-Q1 Other Parts Discussed in Thread: TCAL9539-Q1 , TXE8124-Q1 Tool/software: I would like to have some help with the Functional safety documentation for TXE8116-Q1, the link in the datasheet refers to TCAL9539-Q1 not TXE8116-Q1, could…
Hi Manu,
TCAL9539-Q1 has the input latch feature which would solve the missing status change on MCU power up.
TCA9539A-Q1 is a 5V I2C IO expander, but unfortunately does not latch the input state.
Can the customer consider switching to 5 V SPI using…
Hi Gareth,
TCA6424A is the next best option in QFN.
If you want a leaded 24-bit IO expander, consider using SPI to GPIO with TXE8124-Q1 , there is leaded VSSOP options for this device.
Regards,
Tyler
Hi Sooraj,
This is described in the absolute maximum conditions of the datasheet. Also, I would recommend switching to the TCA9555 if possible.
If the pin is configured as an INPUT, then maximum voltage at the input is 6V.
If the pin is configured…