Part Number: TXS02612 Hello,
in the datasheet of the TXS02612 level translator, a power sequence is given which "should be followed". Can you explain what may happen if the sequence is not exactly followed, e.g. if VCCB ramps shortly before VCCA? Are…
Part Number: TXS02612 Hi team,
The picture below shows the customer's current architecture, the current PCB layout, the FPGA is far from the TXS02612, and the TXS02612 to the SD socket is relatively close. Considering that the signal trace from FPGA…
Part Number: TXS02612 Hello,
I'm trying to do something which is perhaps a little unusual; I'm planning to multiplex SD cards, but share access between two systems with one system only seeing one SD card at a time.
To do this I've employed tw…
Part Number: TXS02612 Other Parts Discussed in Thread: TXS0206A Hi
I want use microcontroller with Wifi module. The communication bus is SDIO in SDR50 or DDR50.
also, my microphone is in 3v3 while the wifi is in 1v8. I want used TXS02612 .
Can you confirm…
Part Number: TXS02612 Dear team
TXS02612 seems to have a switch function. If we only connect to B0, how to connect with B1? Is it floating?
Many thanks
Denny
Part Number: TXS02612 Dear Sirs,
The SD card cannot be found and communication fail with TXS02612 mounted.
Removed IC and direct connect with port A and port B0, everything works fine.
Please help to check is there any problem with the schematics!
Thanks…
Part Number: TXS02612 Dear team
The application is about SDIO bus Level shifter there will be different I/O levels 3.3V or 1.8V In order to unify the design, whether the following schematic diagram is OK? Will it work normally if VCCA and VCCBx are both…
Part Number: TXS02612 Hello,
Pin locations on the package in mechanical drawing pages (21 and 22) are different than rest of the datasheet. Those views in mechanical drawing page 21 &22 are bottom view of the integrated circuit package?
Best Regards…
Part Number: TXS02612 We are currently considering a circuit using TXS02612 to connect Xilinx XC7Z030 -1 FFG 676 I from the MicroSD card slot.
I referred to the circuit diagram of zedboard of xilinx, but there are some parts I don't understand, so I asked…