Part Number: TXU0304-Q1 Hello,
I was going through the datasheet of the TXU0304-Q1 part.
what would be the value of VOH & VOL, it is not mentioned, also Let me the VIH and VIL.
Kindly clarify.
Part Number: TXU0304 Tool/software: Dear Mickael
On the question 3 years ago of Amir :
Amir Eshraghi said:
1. Since TXU0304 have internal pull down, do I still have to pull up, or down chip select of each SPI slaves
Your answer was :
The…
Part Number: TXU0304-Q1 Other Parts Discussed in Thread: TXU0304 , Hi Team,
Is TXU0304-Q1 parametrically equivalent to TXU0304 except that it's automotive qualified?
Thanks!
Roy
Part Number: TXU0304 Tool/software: Dear Team,
We have added TXU0304PWR , this level shifter IC in one of our project for PCM,where as our input Signals IO voltage is 3.3V and Output Signals IO voltage is 1.8V,so requesting you to verify this Schematic…
Part Number: TXU0304 Tool/software: Hello team,
Would Propagation Delay of each channel be somewhat simillar or differ completely across min/max range?
Best Regards, Kei Kuwahara
Part Number: TXU0304 Tool/software: Hi expert,
Customer would like to use TXU0304 for SPI and the SPI will be connected through a cable between a main board and a RF module board. Customer plan to place two TXU0304 one on the main board and another…
Part Number: TXU0304 Other Parts Discussed in Thread: SN74LVC125A Tool/software: how about the data rate when VCCI=VCCO=3.0V ~3.6V? I don't see the condition in d/s.
Application: SPI for Robot
Regards
Brian
Part Number: TXU0304 Tool/software: Regarding version TXU0304RUTR with UQFN 12pin package: How do I know where Pin1 is, when the part is populated? There is just the Device marking 1J6 and some points visible. I do not find the information in the datasheet…
Part Number: TXU0304-Q1 Tool/software: The part has internal pull down for input ports.
If there is no power supply, are those input ports still pull-down?
If there is only one power supply (VCCA, Not VCCB), are those input ports still pull-down?…
Part Number: TXU0304-Q1 Other Parts Discussed in Thread: TXU0304 , SN74AXC4T774 Tool/software: Please recommend several level conversion chips for SPI communication. The maximum communication speed we use is 10MHz
Thank you so much!