Part Number: TXU0304 Hi,
can you tell me what the meaning is "dual-supply noninverting fixed direction voltage level translators"? does it support bi-direction communication from A->B and B->A on 1 channel, saying A1?
or it's one direction…
Yes, the outputs of CMOS devices can be used in parallel.
But increasing the drive strength just to reduce it again with dampening resistors does not make sense. For 5 kbps, you do not need fast edges, so just use a single channel with a resistor that…
Part Number: TXU0304 Hi Support Team
Not getting the info we need on the Ultra Liberian . Can you send us a file for the x2qfn asap for the Allegro PCB Editor 17.4.
See attached file for their question
Thanks
Jeff x2qfn.pptx
Part Number: TXU0304 Hi Team,
Do you have an Altium file for TXU0304DTRR?
If not do you have layout description including all anlges/radians?
Thank you,
Franz
Part Number: TXU0304 Dear, Support Team.
In the table of 7.9 Switching Characteristics, VCCA = 1.8 ± 0.15 V in the datasheet, there is a description of MIN 0.5ns MAX 15ns for tpd (Propagation delay time). Is the MIN to MAX width of this Propagation…
Part Number: TXU0304 Other Parts Discussed in Thread: DAC61416 Hello TI engineers,
We are currently developing a design where we control the DAC61416 (5V logic) with a 3,3 V µC (Teensy 4.1). To achieve SPI communication we need to shift the values to…
Part Number: TXU0304 Other Parts Discussed in Thread: ADS9120 , SN74AXC4T774 Hi team,
My customer looks for level translator which can support >100Mbps at 3.3V=>1.8V. The purpose of this level translator is for connection between 1.8V I/O ADC(ADS9120) and…
Part Number: LSF0204 Other Parts Discussed in Thread: TXU0304 , , LSF0101 , LSF0108
Hi team,
1.may I know what's the comparison between LSF0204 and TXU0304?
does TXU0304 has better driving power?
2. and why LSF0101/2 don't support SPI? I don't see…
Part Number: TXU0304 Other Parts Discussed in Thread: TXU0101 Hello,
Looking at the datasheets of the TXU0304 and the TXU0101 the quiescent current of both devices are identical, is that correct?
Nick
Part Number: TXU0304 Other Parts Discussed in Thread: TXU0101
Hi
First I apologies for asking so many questions regarding SPI logic Translator since I never deal with SPI logic translator.
I have two different SPI salves and I decided to use two of TXU0304…