Part Number: TXU0304 Other Parts Discussed in Thread: TXU0101 Hello,
Looking at the datasheets of the TXU0304 and the TXU0101 the quiescent current of both devices are identical, is that correct?
Nick
Part Number: LSF0204 Other Parts Discussed in Thread: TXU0304 , , LSF0101 , LSF0108
Hi team,
1.may I know what's the comparison between LSF0204 and TXU0304?
does TXU0304 has better driving power?
2. and why LSF0101/2 don't support SPI? I don…
Part Number: TXU0304 Other Parts Discussed in Thread: DAC61416 Hello TI engineers,
We are currently developing a design where we control the DAC61416 (5V logic) with a 3,3 V µC (Teensy 4.1). To achieve SPI communication we need to shift the values to…
Part Number: TXU0304 Hi Team,
A customer is using this part in their design and as per the datasheet the VIL (Min) they are considering as 0V; But they had tested and measured the value VIL = -0.02449; the margin they are getting for this is -0.02449…
Part Number: TXU0304-Q1 hi expert
customer want to use TXU0304-Q1 for SPI buffer and plan to use 1pcs TXU0304-Q1 to carry 12 lane SPI in their long SPI layout. i think it is difficult to evaluate before test on PCB.
how can we have some solution to…
Part Number: TXU0304 Other Parts Discussed in Thread: TXU0101 , TXU0104 , SN74AHC1G125
Hi Team,
Our customer is using a controller and two responders with SPI interface and would like to clarify about the connections of the SPI pins. According to…
Part Number: TXU0304 Other Parts Discussed in Thread: SN65LVDT41 Hi team,
I found TXU0304 can be recommended for SPI interboard communication from this thread .
My customer is looking for SPI board-to-board tranceiver device as well for below requirement…
Part Number: TXU0304
Hi Team,
The input leakage current from the datasheet is 2 μA with 5Mohm internal weak pull down. So the Voltage across the pull down will be quite high and beyond the logic low threshold. Can you help us confirm if the external…
Part Number: TXU0304 Hello,
Currently I am evaluating the TXU0304 by populating it on the 14-24-NL-LOGIC_EVM.
The edges of the signal translating looks good but i see some noise on the steady state voltage. This happens regardless of the frequency…