Part Number: UA78M u78M Linear Regurator, there are two chip (New and Old). Specification is different. (ex. Absolute maximum input voltage, operating temp rank)
How do I distinguish between old and new chips? And how to order new chip regurator ? …
Part Number: UA78M
Hi team,
I would like to ask about the future roadmap for UA78M.
Is there a plan to consolidate UA78M into a new replacement device (new chip)?
If such a consolidation is planned, what is the expected timeline?
This information…
Part Number: UA78M Hello,
A customer is finding a voltage requlator IC which support the followings.
-Vin max. =24V, Vout=10V Fixed, Iou=>0.1A, Tj=-40 ~ +125.
I found UA78M but I couldn't see a part number in the datasheet which supports Tj=-40…
Part Number: UA78M
Hi team,
I have a question about the short-circuit output current specification of the UA78M10.
From my understanding of the datasheet for the legacy chip, when the input voltage (VI) reaches 35 V, the device is judged to…
Part Number: UA78M Tool/software: UA78M05CKCS について調査しております。 データシート 4 Pin Configuration and Functions にKCS0003Bがありません。 ピンアサインの分かる資料を送付ください。 KCS0003B 図面の1から3pin及びTABは以下で合っていますか? 1:INPUT 2:COMMON 3:OUTPUT TAB:COMMON
I am investigating the UA78M05CKCS…
Part Number: UA78M Other Parts Discussed in Thread: TINA-TI , UA78 Hello,
Can you please provide spice model / TINA-TI model of UA78M33CKVURG3.
Regards,
Nikhil Wankhade
Part Number: UA78M Other Parts Discussed in Thread: LM317M Tool/software: Can you provide spice model for UA78M08CKVURG3?
Thank you very much.
Regards,
Petar Stoimenov
Part Number: UA78M Hi team,
My customer is currently using the following products: NJM78M12FA, BA178M12CP-E2, NJM2903D, and BA178M12FP-E2.
As TI alternatives, I believe the following products may be applicable.
Regarding the future availability…
Part Number: UA78M-Q1 Dear TI experts,
I saw about dropout voltage in the datasheet below.
Does it mean that output voltage would be drop If Vin=10V, Vout=5V/350mA so I can only see 3V?
(5V-2V=3V)
But there is little different result in temperature…