Other Parts Discussed in Thread: UC1707-SP , UC1707 I am trying to use UC1707-SP as a gate driver to operate an overvoltage protection system. I am essentially using a zener diode to detect an over voltage event and operate an NMOS to stop current from…
Part Number: UC1707-SP For the UC1707-SP "LCCC" variant you have the pin 19 labled in the table as the "Input A INV" but in the picture it has pin 19 as "INPUT A N.I". It seems to be swapped with pin 20. I want to note your altium pinout seems to align…
Part Number: UC1707-SP Tool/software: DearTeam,
I would like to know regarding the maximum frequency for the IC. It is mentioned high speed in specifications, could you clarify the frequency of it.
Part Number: UC1707-SP Tool/software: Good morning,
Are the particle fluence values available for the "SEL" and "Failure" categories? Unfortunately the LET values alone are of very limited use...
Thank you for your help!
Brent
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 Tool/software: Hello, My customer has a question The UC1707-SP CDIP package has power pins at 14 pin (+Vin) and 8 pins (+Vc), but my customer turned on power to only 14 pins and left 8 pin…
Part Number: UC1707 In response to Mamadou on previous question:
I’ve created a support case for this issue at TI – details:
Number: CS0352694 Contact: Guy Chun First name: Guy Last name: Chun Short description: output of MOSFET driver latching high…
Part Number: UC1707 The Vin and Vc power pins are tied to a +28 VDC Power Supply. Another piece of test equipment caused a -5 Volt Peak (28 VDC to -5 VDC) of duration 10 ns, -3 Volt pulse of duration of 400 ns on the Vin and Vc power pins relative to…
Part Number: UC1707
Hi Team, May I ask for your confirmation? I check datasheet of UC1707 to verify the difference between 5962-8761901EA and UC1707J883B. Yet, I was not able to find its differences. Can you please help me with this? I need to know…
Part Number: UC1707-SP See the discrepancy for pins 19 and 20 in the Pin Functions table versus the Top View. Which one is correct?
The diagram for the FK package (page 3) shows the INPUT A INV on pin 20
The Pin Function Table on the same page shows…