Part Number: UC1707-SP Tool/software: DearTeam,
I would like to know regarding the maximum frequency for the IC. It is mentioned high speed in specifications, could you clarify the frequency of it.
Part Number: UC1707-SP Tool/software: Good morning,
Are the particle fluence values available for the "SEL" and "Failure" categories? Unfortunately the LET values alone are of very limited use...
Thank you for your help!
Brent
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 Tool/software: Hello, My customer has a question The UC1707-SP CDIP package has power pins at 14 pin (+Vin) and 8 pins (+Vc), but my customer turned on power to only 14 pins and left 8…
Part Number: UC1707-SP See the discrepancy for pins 19 and 20 in the Pin Functions table versus the Top View. Which one is correct?
The diagram for the FK package (page 3) shows the INPUT A INV on pin 20
The Pin Function Table on the same page shows…
Part Number: UC1707-SP Hello,
Do you have enhanced low dose rate sensitivity (ELDRS), Displacement Damage Dose (DDD) and Single event latchup (SEL) testing data for the 5962-8761903VFA?
Thanks,
Adam
Part Number: UC1707
Hi Team, May I ask for your confirmation? I check datasheet of UC1707 to verify the difference between 5962-8761901EA and UC1707J883B. Yet, I was not able to find its differences. Can you please help me with this? I need to know differences…
Part Number: UC1707 In response to Mamadou on previous question:
I’ve created a support case for this issue at TI – details:
Number: CS0352694 Contact: Guy Chun First name: Guy Last name: Chun Short description: output of MOSFET driver latching…
Part Number: UC1707-SP Dear Expert .
Good day!
Our customer want to know the 5962-8761903V2A Rad-Tolerant rating , in the datasheet , only describe that
Rad-Tolerant: 50 kRad (Si) for 5962- 8761903VEA, 5962-8761903VFA .
QML-V Qualified, SMD (5962-8761901VEA…
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 , UC3707 , Hi Team,
I think the only difference between them is the "device type" 01 and 03 where 01 means the UC1707 and 03 means UC3707. The difference between UC1707 and UC3707 is…
Part Number: UC1707 We are seeing strange behavior of OUTPUT_A which should follow INPUT_A_NON_INV but latches high when the input is grounded. Has anyone seen this type of latching behavior on the output? Vc=Vin ~15V, OUTPUT_A remains high after INPUT_A_NON_INV…