Part Number: UC1707 The Vin and Vc power pins are tied to a +28 VDC Power Supply. Another piece of test equipment caused a -5 Volt Peak (28 VDC to -5 VDC) of duration 10 ns, -3 Volt pulse of duration of 400 ns on the Vin and Vc power pins relative to ground…
Hi Peter Luong1
Do you have pulse transformer drive circuits and pulse transformer drive chips?
How to prevent VGS misguidance caused by VDS of MOS transistor when using pulse transformer to drive MOS transistor?
Can UC1707 be used to replace EG27324? …
Part Number: UC1707-SP Dear TI experts,
According to SMD document(5962-87619), UC1707-SP have 4 class(M, Q, N,V) according to PIN.
But how can i tell them apart between Class M and Q?
I want to know the class '5962-8761901EA'.
Best regards …
Part Number: UC1707 What is the maximum/minimum voltage on the output pins for the UC1707? We are using the military part number 5962-8761901V2A. We are considering what kinds of diodes we can use for protection on the outputs.
Part Number: UC1707 Working through an anomaly where we had blown driver chips. I suspect that we had the inputs being driven prior to powering on the chips. Is this chip susceptible to latchup in this condition where VCC and Vin+ would have a low impedence…
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 Dear all,
for an aerospace robotics design I do consider using TI's UC1707-SP rad-tolerant gate driver.
In my specific application, gate-driver safety features are important, as these…
Part Number: UC2707 Other Parts Discussed in Thread: UC1707 , UC3707 , UCC27624 Hey team,
Do we have a suitable drop-in/substitute for the UC2707N that's going EOL? I have a customer using this in their design who is concerned.
Thanks in advance!
Ma…
Part Number: UC1707-SP Hi everybody!
I'm using a UC1707-SP Dual-Channel Power Driver (part number 5962-8761901V2A) for a high-reliability, spaceborne system.
In my application, it's driven by a microcontroller, with two 0÷3.3V PWM signals, and drives…
Other Parts Discussed in Thread: LM137QML-SP , TPS7H1210-SEP , TL7700-SEP , UC1707-SP Hello,
Does TI have any similar parts to either the I SL7457SRHF/PROTO, EL7457CSZ, ISL706ARHF/PROTO, or the ISL72991RHF/PROTO? The cross reference tool was not very helpful…
Other Parts Discussed in Thread: MKT-WG16A-MS , MKT-WG10A-MS , SN0020HKH , SN0010HKU , TPS7H1111-SP , TPS7H6003-SP , SN00020FK Looking for mechanical package samples for trim and form setup
Answer:
For our Space Power Ceramic QMLV qualified portfolio of devices…