Part Number: UC1707-SP Tool/software: DearTeam,
I would like to know regarding the maximum frequency for the IC. It is mentioned high speed in specifications, could you clarify the frequency of it.
Part Number: UC1707-SP Tool/software: Good morning,
Are the particle fluence values available for the "SEL" and "Failure" categories? Unfortunately the LET values alone are of very limited use...
Thank you for your help!
Brent
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 Tool/software: Hello, My customer has a question The UC1707-SP CDIP package has power pins at 14 pin (+Vin) and 8 pins (+Vc), but my customer turned on power to only 14 pins and left 8 pin…
Part Number: UC1707-SP See the discrepancy for pins 19 and 20 in the Pin Functions table versus the Top View. Which one is correct?
The diagram for the FK package (page 3) shows the INPUT A INV on pin 20
The Pin Function Table on the same page shows…
Part Number: UC1707-SP Hello,
Do you have enhanced low dose rate sensitivity (ELDRS), Displacement Damage Dose (DDD) and Single event latchup (SEL) testing data for the 5962-8761903VFA?
Thanks,
Adam
Part Number: UC1707-SP Dear Expert .
Good day!
Our customer want to know the 5962-8761903V2A Rad-Tolerant rating , in the datasheet , only describe that
Rad-Tolerant: 50 kRad (Si) for 5962- 8761903VEA, 5962-8761903VFA .
QML-V Qualified, SMD (5962…
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 , UC3707 , Hi Team,
I think the only difference between them is the "device type" 01 and 03 where 01 means the UC1707 and 03 means UC3707. The difference between UC1707 and UC3707 is the…
Part Number: UC1707-SP Dear TI experts,
According to SMD document(5962-87619), UC1707-SP have 4 class(M, Q, N,V) according to PIN.
But how can i tell them apart between Class M and Q?
I want to know the class '5962-8761901EA'.
Best regards…
Part Number: UC1707-SP Other Parts Discussed in Thread: UC1707 Dear all,
for an aerospace robotics design I do consider using TI's UC1707-SP rad-tolerant gate driver.
In my specific application, gate-driver safety features are important, as these…
Part Number: UC1707-SP Hi everybody!
I'm using a UC1707-SP Dual-Channel Power Driver (part number 5962-8761901V2A) for a high-reliability, spaceborne system.
In my application, it's driven by a microcontroller, with two 0÷3.3V PWM signals, and drives…