Part Number: UC1708 Hi,
I am using UC1708L883B and UC1846L88B ics for my power card but I am not able to find the Lead material of these two ics. Able to find the Lead finish in quality and reliability report. Kindly help me regarding this.
Part Number: UC1708-SP Hi Team,
I have a different question on the UC1708-SP. If I’m only using one of the two outputs, what is your recommendation for the INPUT and OUTPUT pins of the unused channel for lowest power consumption?
Thanks!
Connor
Part Number: UC1708-SP Other Parts Discussed in Thread: UC1708 The UC1708 datasheet shows a 10 uF capacitor
in parallel with a 47 uF tantalum capacitor connected from the chip's VCC to ground.
How do I determine what the IC needs in my application…
Part Number: UC1708-SP Hi Team,
Hope you are well!
I am planning to use the UC1708-SP to drive a couple of power MOSFETs at 500 kHz in a converter design. The datasheet only has current supply current draw data for a 2200 pF load switching at 200…
Part Number: UC1708
Hi E2E,
Can you please check if the units for the parameters specified in the table are correct? Is the current in the mA or A range?
Regards, Carlo
Part Number: UC1708 Two questions:
1. I'm operating the UC1708 from 12 volts. I want to keep it permanently enabled. Can I tie the EN pin to 5 volts to keep it permanently enabled? Do you recommend leaving it open in order to permanently enable it?…
Part Number: UC1708-SP Other Parts Discussed in Thread: UC1708 Hello
In my circuit, I use UC1708-SP driver. I added my schematic.
INPUT pin characteristic of UC1708-SP is really interesting. UC1708-SP IN pin behaves like a voltage divider from its…
Hi Kamlesh,
If you disconnect UC1708 and 5K resistor , are you still seeing pulses out of UC1524 at zero duty cycle.
Zero duty cycle implies there are no output pulses. Zero duty cycle relates to where the E/A output crosses the ramp. As this is…
Other Parts Discussed in Thread: UC1825 , UC1708 I have been using UC1524 and UC1708 in my application as shown below.
However, at the time of zero duty ratio, I have seen some pulses at UC1524 and UC1708 output. However, by connecting resistor…