Part Number: UC1708-SP Hi Team,
Hope you are well!
I am planning to use the UC1708-SP to drive a couple of power MOSFETs at 500 kHz in a converter design. The datasheet only has current supply current draw data for a 2200 pF load switching at 200 kHz. …
Part Number: UC1708-SP Hi Team,
I have a different question on the UC1708-SP. If I’m only using one of the two outputs, what is your recommendation for the INPUT and OUTPUT pins of the unused channel for lowest power consumption?
Thanks!
Connor …
Part Number: UC1708
Hi E2E,
Can you please check if the units for the parameters specified in the table are correct? Is the current in the mA or A range?
Regards, Carlo
Part Number: UC1708-SP Other Parts Discussed in Thread: UC1708 The UC1708 datasheet shows a 10 uF capacitor
in parallel with a 47 uF tantalum capacitor connected from the chip's VCC to ground.
How do I determine what the IC needs in my application…
Hey Gg,
Sorry I thought we were talking about the UC1708 device
I would expect that the output of a 1:1 transformer with 15 V signal on the input by 15 V.
The fact you dont see 15 V means there seems to be something wrong with your transformer.
I dont…
Part Number: UC1708-SP I am looking for any type of radiation data for this part. Mostly concerned with TID, but ELDERS and SEE data is also of interest.
Part Number: UC1706 Other Parts Discussed in Thread: UCC27531 , UCC27614 , UC1708-SP , UC1705-SP , UC1709-SP Hi Team,
Can I use UC1706 for designing Buck-Boost converter. Is there a reference design with UC1706
Thanks&Regards
kishan
Part Number: UC1708 Two questions:
1. I'm operating the UC1708 from 12 volts. I want to keep it permanently enabled. Can I tie the EN pin to 5 volts to keep it permanently enabled? Do you recommend leaving it open in order to permanently enable it…
Part Number: UC1708-SP Other Parts Discussed in Thread: UC1708 Hi Team,
I received the following request. Can you help?
##############################
We are nowadays testing the UC1708-SP but we have trouble about it. If you can help on this IC, we can…