Other Parts Discussed in Thread: UC1823A Hi,
Depending on our application, we need to see the performance and some major functions of UC1823A in simulation.
We request you to develop a SPICE model for UC1823A.
Thank you.
Part Number: UC3825A Other Parts Discussed in Thread: UC1823A , , TL494 , UCC28070 Hi Experts,
Good day! As per customer request, I am posting this query to help them find the right device for them.Here is the full details of inquiry below.
If you need more…
On the UC1823A specifically, OUTA and OUTB are operating at F, not F/2. This is based on the note right below the Block Diagram on the datasheet which states "On the UC1823A version, toggles Q and Q are always low". In this case, it would appear…
Part Number: UC1825A-SP Other Parts Discussed in Thread: UC3823B , UC3825B , UC1825A , UC3823A , UC1823A , UC3825A , UC2825A , UC2823B , UC2823A , UC2825B The datasheet of 5962-8768102EA includes a series of chips: UC1823A, UC2823A, UC2823B,UC3823A, UC3823B, UC1825A…
Part Number: UC1825B-SP Other Parts Discussed in Thread: UC1823A-SP , , UC1843B-SP Hello,
TI offers various space-rated "PWM controllers & resonant controllers" ICs. When I look at their datasheets (for instance, for the UC1825B-SP), it says it can support…
Other Parts Discussed in Thread: UC1823A , UCC28700 , LM5085 Hi, I'm looking to design a DC/DC converter that takes 115V to 165V input and steps it down to 100V, 10A output. Are there any reference designs or application notes I can leverage from?
Or…
Other Parts Discussed in Thread: MKT-WG16A-MS , MKT-WG10A-MS , SN0020HKH , SN0010HKU , TPS7H1111-SP , TPS7H6003-SP , SN00020FK Looking for mechanical package samples for trim and form setup
Answer:
For our Space Power Ceramic QMLV qualified portfolio of devices…
Other Parts Discussed in Thread: UC2823A Hi,
At the datasheet of the UC2823A, there are two control techniques defined as VMC and CMC.
At VMC, the RAMP pin is connected to the CT pin.
At CMC, there is a slope compensation loop and some filters.
I want…