Part Number: UC1825A-SP Hello,
Question about the UVLO threshold for the UC1825A-SP. The spec is about 9.2V nominal. What is the coefficient of this threshold over temperature ? Is it increase or decrease with Hot temperature ?
Best Regards,
Jason N…
Part Number: UC1825A Hi TI Support,
I am looking for more detail information regarding the UC1825A (5962-8768012V2A) Error Amplifier parameters variation (Vio, Iio, Ibias).
1) Input offset voltage is listed as 2mV nominal and 10mV max. Is this variation…
Part Number: UC1825A Other Parts Discussed in Thread: UC2825 , UC3842 , UCC28C42 , LM25037 , UCC28250 , UCC28251 , UC2825A Designed a DC-DC converter by using UC2825DW Controller. With this controller met all the electrical parmeters and tested 3 boards. After…
Part Number: UC1825A-SP Hi Team, We have a customer inquiry on how much Voh and Vol vary with temperature to help calculate radiation end points. Please let us know if you have other questions with the customer. Thanks! Jonathan
Part Number: UC1825A-SP I am looking for the tolerance variations (initial tolerance , temperature, aging, radiation) of the 1.25 V internal which connects to the RAMP pin. Beside the 1.25V could impact the current limit, is there any internal parameters…
Part Number: UC1825A Other Parts Discussed in Thread: UC1825 , Hello,
I am looking for the actual oscillation frequency curve over temperature for the PWM UC1825
Thanks
Hi Hong, thank you for sharing the resource.
What are the difference between the UC1825, UC1825A, and UC1825B? The datasheet you share doesn't indicate technical data for the UC1825B but UC1825A.
Does UC1825B has the LEB feature or frequency/deadtime…
Part Number: UC1825A Current limit threshold voltage is spec'd at .95 to 1.05 volts. I am consistently seeing ~ .88X volts, any idea why?? I am using an output hard off as the threshold.
Part Number: UC1825A Other Parts Discussed in Thread: TL431 , UC1825 DC DC converter-- interleaved fly back converter:
Vin= 28-23v
Vout= 5v (Master output @17A)
Two 75W flyback interleaved and working 180 degree out of phase using UC1825A. Feed back loop…